P2P_Client Update_Service() case APP_BLE_DISCOVER_WRITE_DESC Infinite Loop
Hello,
I added a new characteristic to the P2P_Server application that is a, CHAR_PROP_WRITE and GATT_NOTIFY_WRITE_REQ_AND_WAIT_FOR_APPL_RESP = Yes, all other notifications are set to No. The UUID = 50 50. I added the processing of the incoming char and verified that this characteristic shows up in BLE Toolbox and works correctly.
I then edited the P2P_Client uuid.h file and set, P2P_WRITE_CHAR_UUID (0x5050). The characteristic gets discovered in the Update_Service() method and handled in the case APP_BLE_DISCOVER_WRITE_DESC. The handling of the case is the generated code, no changes made.
At this point my application quits working. I discovered the reason by placing a breakpoint inside the case APP_BLE_DISCOVER_WRITE_DESC. It's basically in an infinite loop processing this "event" constantly and no other processing happens.
Is there a reason why adding a write char characteristic would cause this infinite loop situation during the discovery phase?
Kindest regards.