Problem with LoRaWAN_FUOTA_DualCore application for Nucleo-WL55JC1
Hi there, i hope youre doing great!
Im exploring FUOTA over LoRa/LoRaWAN using STM32CubeWL and the Nucleo-WL55JC1
For this purpose im exploring the application (included in STM32CubeWL) "LoRaWAN_FUOTA_DualCore"
I read the 'readme' file to accomplish build and flashing of the board with this application but the build.bat file throws an error
So i decided to compile every project of the full application inside STM32CubeIDE, but in the project 'LoRaWAN_End_Node_DualCore_CM0PLUS' i found a linker error:
... LoRaWAN_End_Node_DualCore_CM0PLUS.elf section `.data' will not fit in region `APPLI_ROM'
...region `APPLI_ROM' overflowed by 272 bytes
Im using STM32CubeIDE v2.0.0 and STM32CubeWL v1.4.0, running on windows 11
Am i doing something wrong?
Any suggestions?