Skip to main content
Visitor II
March 30, 2026
Solved

Reference Design Availability for STM32WLE5JC (Schematics, PCB, RF Layout, Stack-up)

  • March 30, 2026
  • 1 reply
  • 156 views

Hi all,

I am currently working on the design of a custom LoRa/LoRaWAN-based IoT node using the STM32WLE5JCI6TR (bare MCU, not a module), and I am looking for a complete and reliable hardware reference design to follow.

So far, I have identified the following:

  • NUCLEO-WL55JC reference design files (schematics and PCB) from ST, which appear to be the closest official reference (even though it is based on WL55 dual-core variant)

  • Wio-E5 Dev Board from Seeed Studio, which is based on a module and does not expose the RF design details

While these are helpful, I am specifically looking for:

  1. A reference design based directly on STM32WLE5JC (or very close variant)

  2. Complete design files including:

    • Full schematics

    • PCB layout files

    • RF matching network implementation

    • Antenna routing

    • PCB stack-up / layer information

Since RF design (matching, impedance control, grounding, etc.) is quite sensitive, having a proven reference is critical.

Additionally, I would like to know:

:backhand_index_pointing_right: Are there any open-source or freely available reference designs based on STM32WLE5JC that include full PCB and RF layout details?

Any guidance, shared designs, or recommendations would be greatly appreciated.

Thanks in advance!

Best answer by Imen.D

Hello @Vimukthi-Wathudura and Welcome to the Community,

Please refer to the following resources:

STM32WL5x-Ex wireless MCU lines - Wireless MCUs System-on-Chip Long-range communications

Data brief - STDES-WL5xxxxx - Reference designs for STM32WL5x and STM32WLEx microcontrollers

1 reply

Imen.DBest answer
Technical Moderator
March 30, 2026
"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"