Skip to main content
kcire L.
Associate III
March 22, 2022
Solved

RTC current time in milliseconds (display in 6 byte hex)

  • March 22, 2022
  • 3 replies
  • 5419 views

Hello,

I am using an STM32WB55 and am trying to figure out how to get the current time including milliseconds using an RTC and display that time in 6 byte hex format.

I would most likely call the GetTime() based of a millisecond timer if that is the most efficient way to do it.

For example I would like the time to return like this (0x017FB1731312)

Any help or example on this would really be appreciated.

Thanks in advance!

Best answer by Peter BENSCH

This won't work because you can't get millisecond information from the RTC if you have a 32.768kHz (2^15 Hz) crystal connected, which can't be divided down to 1kHz using an integer value.

There is only the counting down subsecond counter RTC_SSR, which is by default set to 256 at 32.768kHz.

If you want millisecond information, it makes most sense to use a timer and process this information with it. In principle, you can also use the systick timer, which triggers an interrupt every 1ms by default.

However, I am not aware of a ready-made proposal for your requirements for any of the options.

Does it answer your question?

Regards

/Peter

3 replies

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
March 22, 2022

This won't work because you can't get millisecond information from the RTC if you have a 32.768kHz (2^15 Hz) crystal connected, which can't be divided down to 1kHz using an integer value.

There is only the counting down subsecond counter RTC_SSR, which is by default set to 256 at 32.768kHz.

If you want millisecond information, it makes most sense to use a timer and process this information with it. In principle, you can also use the systick timer, which triggers an interrupt every 1ms by default.

However, I am not aware of a ready-made proposal for your requirements for any of the options.

Does it answer your question?

Regards

/Peter

SAsse.1
Visitor II
April 25, 2023

What I am using is one of the 2 RTC Alarm that I configure for 1 sec call back. In the call back function I clear a public variable. That variable gets incremented in the 1 ms SysTick interrupt.

The reason we need to use SyTick is to get milliseconds counter.

The reason we need to use RTC is to synchronize the counting of milllisecond above to the change in seconds.

Note: I use: Counter %= 1000; // to make sure millisec always fall in [0..999] range

Explorer II
January 21, 2025

I did some simple research on this issue. When trying to get milliseconds from RTC, the resolution will not be very useful. It's about 4ms. Or more precisely 3.90625ms. 

 

 

// execution interval 1ms
INTERVAL_BLOCK(gpTimer0, 1)
{
 HAL_RTC_GetTime(&hrtc,&RTC_Time,RTC_FORMAT_BCD);
 HAL_RTC_GetDate(&hrtc,&RTC_Date,RTC_FORMAT_BCD);

 printf("RTC_Time: %x:%x:%x-%li(%li)| Date:%x.%x.20%x \r\n", 
 RTC_Time.Hours, \
 RTC_Time.Minutes, \
 RTC_Time.Seconds, \
 (RTC_Time.SecondFraction*1000 -RTC_Time.SubSeconds*1000)/(RTC_Time.SecondFraction+1) 
, \
 RTC_Time.SubSeconds, \
 RTC_Date.Date, \
 RTC_Date.Month, \
 RTC_Date.Year);
}

 

 

 And the result looks like this:

 

 

RTC_Time: 0:0:0-101(229)| Date:21.1.2024 
RTC_Time: 0:0:0-101(229)| Date:21.1.2024 
RTC_Time: 0:0:0-101(229)| Date:21.1.2024 
RTC_Time: 0:0:0-101(229)| Date:21.1.2024 
RTC_Time: 0:0:0-105(228)| Date:21.1.2024 
RTC_Time: 0:0:0-105(228)| Date:21.1.2024 
RTC_Time: 0:0:0-105(228)| Date:21.1.2024 
RTC_Time: 0:0:0-105(228)| Date:21.1.2024 
RTC_Time: 0:0:0-109(227)| Date:21.1.2024 
RTC_Time: 0:0:0-109(227)| Date:21.1.2024 
RTC_Time: 0:0:0-109(227)| Date:21.1.2024 
RTC_Time: 0:0:0-109(227)| Date:21.1.2024 

 

 

You can try to set the 7bit asynchronous prescaler (PREDIV_A) to 31 (0x1F) and the 15bit synchronous prescaler (PREDIV_S) to 1023 (0x3FF). In this case, the resolution will be 0.976563ms. This is quite close, but still not exactly 1ms.

That's why sometimes you will encounter such glitches:

 

 

RTC_Time: 0:0:0-475(537)| Date:21.1.2024 
RTC_Time: 0:0:0-476(536)| Date:21.1.2024 
RTC_Time: 0:0:0-477(535)| Date:21.1.2024 
RTC_Time: 0:0:0-478(534)| Date:21.1.2024 <<<<< ERROR
RTC_Time: 0:0:0-478(533)| Date:21.1.2024 <<<<< ERROR
RTC_Time: 0:0:0-479(532)| Date:21.1.2024 
RTC_Time: 0:0:0-480(531)| Date:21.1.2024 
RTC_Time: 0:0:0-481(530)| Date:21.1.2024