Sequencer stop when LPTIM1 Started
I am using the LoRaWAN_End_node application. The application was working fine until I integrated the Low Power sample code. The Sequencer appears to stop working (I suspect the timers are not working). If I do not do add MX_LPTIM1_Init() in main everything appears to work. The problem is without the LPTIM1 I can not wake up the processor.
HAL_LPTIM_Counter_Start_IT(&hlptim1,(2000 * LSI_VALUE / 1000));
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
Thanks for the help.