Setting SC_KEY_TYPE to debug mode fails in STM32WB55
Hello,
I want to enable the secure connection key type as 'DEBUG' in STM32WB55 with my custom setup. The cube IDE does not allow this setting in the configuration of .ioc file. I followed this tutorial and added the following line in my code inside the definition of Ble_Hci_Gap_Gatt_Init() function, but it returns with error code 0x12 (Invalid HCI parameters). What am I missing here?
static const uint8_t SC_KEY_TYPE_DEBUG = 1;
static const uint8_t SC_KEY_TYPE_NORMAL = 0;
ret = aci_hal_write_config_data(0x35U, 1, (uint8_t*)&SC_KEY_TYPE_DEBUG);
if (ret != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG(" Fail : aci_hal_write_config_data command - CONFIG_DATA_SC_KEY_TYPE_OFFSET, result: 0x%x \n", ret);
}
else
{
APP_DBG_MSG(" Success: aci_hal_write_config_data command - CONFIG_DATA_SC_KEY_TYPE_OFFSET\n");
}I am also following AN5270 for development, and the offset to set SC_KEY_TYPE seems to be correct.

This is what I am seeing when I run the code:

I made sure that CFG_SC_SUPPORT is set to 0x02 (supported and mandatory). What am I missing here?
Any help is appreciated!