Skip to main content
Visitor II
December 4, 2025
Question

ST67W External/Internal CoExistence Support

  • December 4, 2025
  • 1 reply
  • 499 views

Hello,

I am designing a Matter/Zigbee Gateway using an STM32U5 as the host. My planned architecture includes:

  1. ST67W: Handling Wi-Fi and Thread (Matter over Wi-Fi/Thread).

  2. STM32WBA (or similar): Handling Zigbee (Matter Bridge logic).

I have two specific questions regarding the ST67W's coexistence capabilities:

  1. Internal Coexistence: Does the ST67W natively support concurrent operation of Wi-Fi and Thread simultaneously without external hardware arbitration?

  2. External PTA Support: Does the ST67W expose 3-wire PTA pins (Request/Priority/Grant) to manage coexistence with an external 802.15.4 radio (e.g., the STM32WBA running Zigbee)?

Basically, I need to confirm if it supports a "Hybrid Coexistence" setup where it manages internal Wi-Fi/Thread traffic while acting as a PTA Arbiter for an external Zigbee MCU.

Thanks in advance.

1 reply

EPASZ.1
ST Employee
December 4, 2025

Unfortunately, at the moment the module does not expose Thread functionality to the host. So question 1 is not completely applicable.

Similarly for question 2 - PTA is not supported by the HW.