Skip to main content
Visitor II
July 7, 2025
Solved

STM32 MCU model shortlisting for Making RC remote

  • July 7, 2025
  • 2 replies
  • 277 views

Hi everyone,

  1. which type of stm32 microcontroller is best fit for following operations
  2. for building rc remote of 8 channel and more
  3. low cost
  4. low power consumption
  5. high-speed rf communication and easy integrate with RF chip using SPI port
  6. easy to design and develop
  7. 10-bit ADC
  8. low voltage
  9. display interference
  10. RTC
Best answer by STTwo-32

Hello @Palnerve and welcome to the ST Community.

I suggest you use the ST-MCU-FINDER-PC - STM32 and STM8 product finder for desktops - STMicroelectronics standalone or the STM32CubeMX integrated version:

STTwo32_0-1751894826464.png

Using the filters, you can select the MCU you are looking for according to the filters you select.

Best Regards.

STTwo-32

2 replies

STTwo-32
STTwo-32Best answer
Technical Moderator
July 7, 2025

Hello @Palnerve and welcome to the ST Community.

I suggest you use the ST-MCU-FINDER-PC - STM32 and STM8 product finder for desktops - STMicroelectronics standalone or the STM32CubeMX integrated version:

STTwo32_0-1751894826464.png

Using the filters, you can select the MCU you are looking for according to the filters you select.

Best Regards.

STTwo-32

TDK
Super User
July 8, 2025

> easy to design and develop

No MCUs fit this description, at least not for a project with SPI/RF/display

"If you feel a post has answered your question, please click ""Accept as Solution""."