Skip to main content
Associate III
March 11, 2025
Solved

STM32cubemonitorRF - 'Get RSSI' disabled

  • March 11, 2025
  • 2 replies
  • 773 views

Hello

i'm using STM32WB05KZ (nucleo board) : Nucleo-WB05KZ with STM32CubemonitorRF

Please why here i can't select  "Get RSSI" , it's locked ?

ljm_0-1741690654359.png

and other question how can i modifie the outpout power (TX) of the antenna ( dBm) ? 

thank you 

Best answer by STTwo-32

Hello @ljm 

The Get RSSI option is locked due to the Firmware implementation on the STM32WB0, the ACI_HAL_READ_RSSI command is not supported.

For the second question, if you are testing on a transmitter, you can set the PA Level you want here:

STTwo32_0-1741774312154.png

Best Regards.

STTwo-32

 

2 replies

STTwo-32
STTwo-32Best answer
Technical Moderator
March 12, 2025

Hello @ljm 

The Get RSSI option is locked due to the Firmware implementation on the STM32WB0, the ACI_HAL_READ_RSSI command is not supported.

For the second question, if you are testing on a transmitter, you can set the PA Level you want here:

STTwo32_0-1741774312154.png

Best Regards.

STTwo-32

 

ljmAuthor
Associate III
March 12, 2025

hello

thanks for replying.

for "Get RSSI" means there is no solution to get the RSSI value ?

i do the some in mode transmission, i get the number of packets but there is no value for the rssi : 

ljm_0-1741775471767.png

thanks

STTwo-32
Technical Moderator
March 12, 2025

For the STM32WB0, you can't get the RSSI using the STM32CubeMonitorRF. 

 

Andrew Neil
Super User
March 12, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.