STM32CubeMX - Programming an BLE LP device (WB07CC)
With the introduction of the new STM32WB07 MCUs in the STM32CubeMX software, the BLEMGR Middleware has also been added. Within this Middleware, it is supposed to be possible to programm BLE Low Power (LP) devices.
However, there is a lack of documentation and examples on how to work with the code generated by CubeMX for programming LP devices. While I have worked with previous LP devices using examples (e.g., from the STM32WB Navigator App and the specific examples for the STM32WB07CC evaluation board), the situation is different with the CubeMX-generated projects.
In past examples, the initialization process involved calling a BLE_STACK_Init() function, which initializes the BLE stack as well as initalizing other components such as the PKA, AES, and NVM Manage. Unfortunately, these functions, are missing when generating code through CubeMX for the WB07CC.
I attempted to initialize the BLE stack using the available functions, but consistently encountered a timeout error.
It would be highly beneficial to have some guidance or examples that demonstrate how to properly utilize the CubeMX-generated code for an LP device, particularly when programming the STM32WB07CC chip directly (without an external controller). It’s worth noting that when creating a project in CubeMX, the use of an intermediary controller seems non-optional, which adds to the challenge.
Any detailed examples or best practices for configuring and initializing the BLE stack for the WB07CC using CubeMX would be greatly appreciated.