Skip to main content
Associate II
February 2, 2026
Question

[STM32WB55] Random "Silent" Disconnection & Reconnection Loop. FW V1.24.

  • February 2, 2026
  • 0 replies
  • 154 views

Hello everyone,

I am facing severe stability issues with a Nucleo-WB55RG project generated via STM32CubeMX (FW Package V1.24.0).

The Core Problem: The device advertises and connects, but suffers from random "Silent" Disconnections (no event generated) - connection loops and eventually complete silent (advertisement doesnt start after disconnection). This happens in multiple scenarios, including simple idle connections and bonding attempts.

Detailed Scenarios:

1. Scenario A: Idle Connection (Without Bonding)

  • I connect using the ST BLE Toolbox app and leave it idle.

  • Behavior: After a random period (non-uniform time), the device automatically disconnects, reconnects, and enters a loop.

  • Observation: Even without initiating bonding, the link is unstable.

2. Scenario B: Pairing via Android Bluetooth Settings

  • I go to Android Settings > Bluetooth and tap the device to Pair.

  • Behavior: The phone displays "Pairing..." indefinitely.

  • Observation: The UART logs show "BLE Connected", but the handshake never completes. After a short while, the device silently disconnects and restarts the advertisement loop.

3. Scenario C: Bonding via ST BLE Toolbox

  • I connect and click the "Bond" button in the app.

  • Behavior: The app shows a Bonding, followed by the same silent disconnection.

Key Technical Observations:

  • Silent Failure: When these automatic disconnects happen (in any scenario above), my application DOES NOT receive the HCI_DISCONNECTION_COMPLETE_EVT.

  • Manual Disconnect Works: If I manually disconnect from the App before the crash, the Event IS received correctly.

  • Data Transfer: I haven't been able to verify data transfer reliability because the connection drops too frequently.

Setup Details:

  • Board: Nucleo-WB55RG

  • FW: V1.24.0 (Binaries updated via CubeProgrammer).

  • Security: Just Works (NoInputNoOutput), Bonding Enabled.

  • Clock: Default CubeMX configuration (LSE: 32.768kHz).

Questions:

  1. Why does the M0+ stack drop the link without triggering a Disconnection Event to the M4 core?

  2. Could this random instability be related to LSE Clock accuracy/configuration?

  3. Has anyone successfully used "Just Works" bonding on FW 1.24 without these hangs?


I have attached IOC file for reference, also, i am currently using generated code only, not even started application logic. 

Any insights would be helpful.