STM32WB5MM-DK, connecting to Tuya gateway with zigbee, part 2
- January 19, 2024
- 4 replies
- 9231 views
Hello,
I have still connection problem to Tuya gateway. Simple OnOff application can connect to Tuya gateway, but when I try to connect STM32WB5MM-DK as a temperature sensor, connection fails.
Connection to Tuya gateway succeeds with STM32WB5MM-DK example OnOff_Server_Coordinator and On/Off button comes visible on SmartLife app. But with temperature sensor application connection won't work. The application things that it has succeed to connect, but nothing comes visible in SmartLife app. Little display shows "Join ok". According to Wireshark logs, temperature sensor won't reply to gateway's read attributes request where it wants to read basic attributes:
Command: Read Attributes (0x00)
Attribute: Manufacturer Name (0x0004)
Attribute: ZCL Version (0x0000)
Attribute: Application Version (0x0001)
Attribute: Model Identifier (0x0005)
Attribute: Power Source (0x0007)
Attribute: Unknown (0xfffe)
OnOff application responds for that, but not quite like should. Anyway connection succeed.
Connection shoud go according to that specification:
【Zigbee Popular Science Series】 - 3 Network Access Process - Tuya Developer Forum (tuyaos.com)
I attached three Wireshark log; WB5MM_OnOff__Server_Coord, WB5MM_TempMeas_Server_Coord and Nedis_capture. In both Server_Coord applications, I changed starttype --> join and also channel change to WPAN_2400MHZ.
I'am not shure is that the reason why connection fail, but this is at least first difference.