Associate II
July 29, 2025
Solved
STM32WB5MMG: Cube Monitor RF refuses to connect
- July 29, 2025
- 9 replies
- 777 views
We are using an STM32WB5MMG in a product, We needed to run a few BLE tests for compliance needs and came across the BLE transparent mode to help with BLE tests.
In accordance with the ReadMe under BLE_TransparentMode inside STM32WB5MM-DK, we have undertaken the following steps
- Updated FUS to stm32wb5x_FUS_fw.bin at 0x080EE000
- Updated soft device with stm32wb5x_BLE_Stack_full_extended_fw.bin to 0x080C7000
- Modified BLE transparent Mode to change USART pins being used to PA9 and PA10 though Cube MX

Updated FUS and Stack

Updated VCP_TX and VCP_RX
The CubeMonitor-RF software refuses to connect with the device however

Unable to connect
No changes are done to the transparent mode example with the exception of UART pin update. ioc file PDF attached