STM32WBA52 ADC Maximum Clock Frequency & Max Sample Rate at 12-Bit Resolution
Hi Enthusiastic,
MCU: STM32WBA52CGU6
STM32CubeMX: 6.9.0
STM32CubeIDE: 1.12.0
Toolchain - GNU Tools for STM32: 11.3rel1
SDK - STM32CubeWBA: V1.1.1
Query related to maximum ADC-Clock-Frequency & maximum sample-per-second with 12-Bit Resolution ADC.
I have go through Datasheet, Reference-Manual & ST-Community,
As per mentioned and gathered information:
1. Not clearly Maximum value for ADC-Clock-Frequency in any source.
2. As per datasheet: DS14127 Rev 7: Page 47:
https://www.st.com/resource/en/datasheet/stm32wba52ce.pdf
Note: The ADC4 analog block clock frequency after the ADC4 prescaler must be between 140 kHz and 55 MHz.
3. As per datasheet: DS14127 Rev 7: Page 45: Table 14:
https://www.st.com/resource/en/datasheet/stm32wba52ce.pdf
Maximum sampling speed for 12-bit resolution: 2.5 Msps
4. As per Reference Manual RM0493 Rev 5: Page 636:
https://www.st.com/resource/en/reference_manual/rm0493-multiprotocol-wireless-bluetooth-lowenergy-and-ieee802154-stm32wba5xxx-armbased-32bit-mcus-stmicroelectronics.pdf
tCONV = tSMPL + tSAR = [1.5 |min + 12.5 |12bit] x tADC_CLK
tCONV = tSMPL + tSAR = 42.9 ns |min + 357.1 ns |12bit = 0.400 µs |min (for fADC_CLK = 35 MHz)
5. In above equation taken, fADC_CLK = 35 MHz,
As per Point-2 above, possible to feed maximum fADC_CLK = 55 MHz,
As per Point-4 above, using fADC_CLK = 55 MHz, can achieve tCONV = 3.928 Msps.
6. Note that with trial of set fADC_CLK = 55 MHz, successfully get proper ADC readings.
7. When tried with 70 MHz, successfully get proper ADC readings.
Root question is that, is it fine to use fADC_CLK = 70 MHZ, because datasheet mentioned not but practically looks working fine, and what is real maximum allowable fADC_CLK and maximum SMPS?
Thanks.