Skip to main content
Associate II
May 23, 2025
Solved

STM32WL33 data coding

  • May 23, 2025
  • 1 reply
  • 416 views

I'm transmitting a custom packet by the NUCLEO-WL33CC2 and I'm receiving the pachet by a different harware that use the SI4460 tranceiver from Silabs. In the receiver board I receive the pachet, but the byte are completely differents than the byte I sent. Look like as the STM32WL33 have applied a coding, but I do non have applied any coding on the transmetter.

This my init code on the trasmetter:

static void MX_MRSUBG_Init(void)
{

 /* USER CODE BEGIN MRSUBG_Init 0 */

 /* USER CODE END MRSUBG_Init 0 */

 /* USER CODE BEGIN MRSUBG_Init 1 */

 /* USER CODE END MRSUBG_Init 1 */

 /** Configures the radio parameters
 */
 MRSUBG_RadioInitStruct.lFrequencyBase = 433920000;
 MRSUBG_RadioInitStruct.xModulationSelect = MOD_2GFSK1;
 MRSUBG_RadioInitStruct.lDatarate = 40000;
 MRSUBG_RadioInitStruct.lFreqDev = 25000;
 MRSUBG_RadioInitStruct.lBandwidth = 100000;
 MRSUBG_RadioInitStruct.dsssExp = 0;
 MRSUBG_RadioInitStruct.outputPower = 14;
 MRSUBG_RadioInitStruct.PADrvMode = PA_DRV_TX_HP;
 HAL_MRSubG_Init(&MRSUBG_RadioInitStruct);

 /** Configures the packet parameters
 */
 MRSUBG_PacketSettingsStruct.PreambleLength = 64;
 MRSUBG_PacketSettingsStruct.PostambleLength = 0;
 MRSUBG_PacketSettingsStruct.SyncLength = 16;
 MRSUBG_PacketSettingsStruct.SyncWord = 0x2DD48888;
 MRSUBG_PacketSettingsStruct.FixVarLength = FIXED;
 MRSUBG_PacketSettingsStruct.PreambleSequence = PRE_SEQ_1010;
 MRSUBG_PacketSettingsStruct.PostambleSequence = POST_SEQ_0101;
 MRSUBG_PacketSettingsStruct.CrcMode = PKT_NO_CRC;
 MRSUBG_PacketSettingsStruct.Coding = CODING_NONE;
 MRSUBG_PacketSettingsStruct.DataWhitening = DISABLE;
 MRSUBG_PacketSettingsStruct.LengthWidth = BYTE_LEN_1;
 MRSUBG_PacketSettingsStruct.SyncPresent = ENABLE;
 HAL_MRSubG_PacketBasicInit(&MRSUBG_PacketSettingsStruct);
 /* USER CODE BEGIN MRSUBG_Init 2 */

 /* USER CODE END MRSUBG_Init 2 */

}

This my transmition instructions:

uint8_t tx_data[MSG_SIZE]={0x10, 0x40, 0x90, 0x00, 0x00, 0x35, 0x0D, 0x00, 0x03, 0x00, 0x00, 0x00, 0x00, 0x00, 0x1e, 0xe1 };
	__HAL_MRSUBG_STROBE_CMD(CMD_SABORT);


	/* wait for SABORT... */
	while ((__HAL_MRSUBG_GET_RFSEQ_IRQ_STATUS() & MR_SUBG_GLOB_STATUS_RFSEQ_IRQ_STATUS_SABORT_DONE_F) == 0) {};
	__HAL_MRSUBG_CLEAR_RFSEQ_IRQ_FLAG(MR_SUBG_GLOB_STATUS_RFSEQ_IRQ_STATUS_SABORT_DONE_F);

	/* Set the pointer to the data buffer */
	HAL_MRSubG_PktBasicSetPayloadLength(MSG_SIZE);
	__HAL_MRSUBG_SET_DATABUFFER0_POINTER((uint32_t)&tx_data);

	/* Send the TX command */
	__HAL_MRSUBG_STROBE_CMD(CMD_TX);

 in the receiver I have these data:

sbelcatronic_0-1748004288054.png

How can I solve?

I have tested the NUCLEO-WL33CC2 and my receiver by the STM32CubeWiSE-RadioExplorer and I can send and receve the correct packet.

Thank you.

Best answer by sbelcatronic

I solved the problem! Was a wrong configuration in SyncLenght. I wrote

MRSUBG_PacketSettingsStruct.SyncLength = 16;

 But the reference manual wrote:

sbelcatronic_0-1748412472548.png

so to get 16 bits in syncronization word I need to write the SyncLenght parameter 15 value. So simply writing

MRSUBG_PacketSettingsStruct.SyncLength = 15;

  solve the problem.

 

1 reply

sbelcatronicAuthorBest answer
Associate II
May 28, 2025

I solved the problem! Was a wrong configuration in SyncLenght. I wrote

MRSUBG_PacketSettingsStruct.SyncLength = 16;

 But the reference manual wrote:

sbelcatronic_0-1748412472548.png

so to get 16 bits in syncronization word I need to write the SyncLenght parameter 15 value. So simply writing

MRSUBG_PacketSettingsStruct.SyncLength = 15;

  solve the problem.