STM32WL33 Receive Interrupt Stops Firing after Low RSSI signals and doesn't recover
I'm using a STM32WL33 on 2 separate custom PCBs. I have one of them being a transmitter only, and I have verified that the transmitter consistently transmits when the keyfob button(s) are pressed (using one of the examples on a Nucleo CC2 board to verify)
I'm having issues with the receiver ceasing to recover after receiving a low-RSSI signal. As long as the signal strength is reasonable, the HAL_MRSubG_IRQ_Callback executes, and resumes reception without issue. If it receives a packet that is of questionable RSSI (either too far away with the keyfob or wrapping the keyfob in aluminum foil to keep my step count down :) ), the HAL_MRSubG_IRQ_Callback doesn't execute at all once the RSSI is back to the original level, and requires a power cycle to recover. The main loop continues to operate, it's just that the interrupt ceases to fire! I have observed the same thing on the Nucleo CC2 PCB as well using the Chat example. A reboot solves the issue there, as well.
Any insight is appreciated! In the meantime, I'm going to start debugging some register contents and see if somehow the interrupt is getting disabled.
Thanks!
Below are the relevant code snippets:
/** Configures the radio parameters
*/
MRSUBG_RadioInitStruct.lFrequencyBase = 433000000;
MRSUBG_RadioInitStruct.xModulationSelect = MOD_2FSK;
MRSUBG_RadioInitStruct.lDatarate = 38400;
MRSUBG_RadioInitStruct.lFreqDev = 20000;
MRSUBG_RadioInitStruct.lBandwidth = 100000;
MRSUBG_RadioInitStruct.dsssExp = 0;
MRSUBG_RadioInitStruct.outputPower = 14;
MRSUBG_RadioInitStruct.PADrvMode = PA_DRV_TX_HP;
HAL_MRSubG_Init(&MRSUBG_RadioInitStruct);
/** Configures the packet parameters
*/
MRSUBG_PacketSettingsStruct.PreambleLength = 16;
MRSUBG_PacketSettingsStruct.PostambleLength = 0;
MRSUBG_PacketSettingsStruct.SyncLength = 31;
MRSUBG_PacketSettingsStruct.SyncWord = 0x88888888;
MRSUBG_PacketSettingsStruct.FixVarLength = VARIABLE;
MRSUBG_PacketSettingsStruct.PreambleSequence = PRE_SEQ_0101;
MRSUBG_PacketSettingsStruct.PostambleSequence = POST_SEQ_0101;
MRSUBG_PacketSettingsStruct.CrcMode = PKT_CRC_MODE_8BITS;
MRSUBG_PacketSettingsStruct.Coding = CODING_NONE;
MRSUBG_PacketSettingsStruct.DataWhitening = ENABLE;
MRSUBG_PacketSettingsStruct.LengthWidth = BYTE_LEN_1;
MRSUBG_PacketSettingsStruct.SyncPresent = ENABLE;
HAL_MRSubG_PacketBasicInit(&MRSUBG_PacketSettingsStruct);
/* USER CODE BEGIN MRSUBG_Init 2 */void protocol_init(void)
{
HAL_MRSubG_PktBasicSetPayloadLength(sizeof(rx_packet_t));
__HAL_MRSUBG_SET_RFSEQ_IRQ_ENABLE(MR_SUBG_GLOB_DYNAMIC_RFSEQ_IRQ_ENABLE_RX_OK_E | MR_SUBG_GLOB_DYNAMIC_RFSEQ_IRQ_ENABLE_TX_DONE_E);
HAL_NVIC_EnableIRQ(MR_SUBG_IRQn);
__HAL_MRSUBG_SET_DATABUFFER0_POINTER((uint32_t)&rx_packet_isr);
__HAL_MRSUBG_STROBE_CMD(CMD_RX);
}void HAL_MRSubG_IRQ_Callback(void){
uint32_t irq;
uint8_t *ptr = (uint8_t *)&rx_packet_isr;
irq = __HAL_MRSUBG_GET_RFSEQ_IRQ_STATUS();
if (irq & MR_SUBG_GLOB_STATUS_RFSEQ_IRQ_STATUS_RX_OK_F) {
/* Clear the IRQ flag */
__HAL_MRSUBG_CLEAR_RFSEQ_IRQ_FLAG(MR_SUBG_GLOB_STATUS_RFSEQ_IRQ_STATUS_RX_OK_F);
uint16_t rxBytes = __HAL_MRSUBG_GET_DATABUFFER_COUNT();
if(ptr[rxBytes-1] == (uint8_t)HAL_CRC_Calculate(&hcrc, (uint32_t *)&rx_packet_isr, rxBytes-1))
{
printf("RX:\t");
for(uint8_t i = 0; i<rxBytes; i++)
{
printf("%02X ",ptr[i]);
}
printf("\r\n");
}
__HAL_MRSUBG_SET_DATABUFFER0_POINTER((uint32_t)&rx_packet_isr);
__HAL_MRSUBG_STROBE_CMD(CMD_RX);
}
if (irq & MR_SUBG_GLOB_STATUS_RFSEQ_IRQ_STATUS_TX_DONE_F ) {
/* Clear the IRQ flag */
__HAL_MRSUBG_CLEAR_RFSEQ_IRQ_FLAG(MR_SUBG_GLOB_STATUS_RFSEQ_IRQ_STATUS_TX_DONE_F);
/* set the tx_done_flag to manage the event in the main() */
tx_done_flag = TRUE;
}
}