STM32WL55 doesn't work with 1.8V
Hi,
I am working on a LoRa application with the STM32WL5MOC module which features the STM32WL55JC microcontroller. According to the datasheet, this module is compatible with a voltage level as low as 1.8V.
I am using the STM32CubeWL MCU Package for the firmware, and I have configured the Low Power (LP) mode for a 14dBm transmission power. However, the board stops functioning whenever the voltage drops below 2.05V.
Has anyone encountered a similar issue or have any suggestions on how to address this?
Thanks in advance!