Skip to main content
Associate
February 25, 2025
Question

[STM32WL55JC1] - How to migrate from LoRaWAN EndNode to LoRa FUOTA example?

  • February 25, 2025
  • 1 reply
  • 513 views

Hello,

I have developed a LoRa application based on the LoRaWAN EndNode example, with some custom code and using the .ioc configuration. I am working on the Nucleo board STM32WL55JC1.

Now, I would like to migrate my application to the LoRa End Node FUOTA example while keeping my existing development. However, I am unsure about the best approach to achieve this.

Should I replace the LoRa End Node project inside the FUOTA example (though I assume I will miss some FUOTA-specific classes and functions)?
Or should I integrate the additional FUOTA-related projects (KMS_blob, EWARM,BFU, SECoreBin,Linker ...) around my existing LoRa application?

Any guidance or best practices would be greatly appreciated.

Thanks!

1 reply

STTwo-32
Technical Moderator
March 24, 2025

Hello @SamyHaouaraUTC 

What I suggest you is to try the same implementation as on the example LoRaWAN_FUOTA available under STM32Cube_FW_WL_V1.3.1\Projects\NUCLEO-WL55JC\Applications.

Best Regards.

STTwo-32