STM32WL5MOC Delevopment Issues
Hello everyone,
I'm trying to setup a STL32CubeIDE project with a custom STM32WL5MOCH6 MCU. I managed to test if the board is alive with a simple hello world debug print on SWV and there's no issues.
The problem starts when I enable the LORAWAN middleware (EndNode Skeleton Application):

For this i have to enable IPCC, ADC and RTC :



But when i generate the code and build the project i get those errors :
- CM4 :
../Core/Src/usart_if.c:107:3: warning: implicit declaration of function 'MX_DMA_Init'; did you mean 'MX_RTC_Init'? [-Wimplicit-function-declaration]
107 | MX_DMA_Init();
| ^~~~~~~~~~~
| MX_RTC_Init
../Core/Src/usart_if.c:108:3: warning: implicit declaration of function 'MX_USART1_UART_Init' [-Wimplicit-function-declaration]
108 | MX_USART1_UART_Init();
| ^~~~~~~~~~~~~~~~~~~
arm-none-eabi-gcc -o "aerosentinel_echo_CM4.elf" @"objects.list" -mcpu=cortex-m4 -T"C:\Users\Yassine DEHHANI\Documents\aerosentinel-echo\CM4\STM32WL5MOCHX_FLASH.ld" --specs=nosys.specs -Wl,-Map="aerosentinel_echo_CM4.map" -Wl,--gc-sections -static --specs=nano.specs -mfloat-abi=soft -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
C:/ST/STM32CubeIDE_1.15.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Core/Src/timer_if.o:C:/Users/Yassine DEHHANI/Documents/aerosentinel-echo/CM4/Debug/../Core/Src/timer_if.c:36: multiple definition of `hrtc'; ./Core/Src/main.o:C:/Users/Yassine DEHHANI/Documents/aerosentinel-echo/CM4/Debug/../Core/Src/main.c:48: first defined here
C:/ST/STM32CubeIDE_1.15.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Core/Src/usart_if.o: in function `vcom_Init':
C:/Users/Yassine DEHHANI/Documents/aerosentinel-echo/CM4/Debug/../Core/Src/usart_if.c:107: undefined reference to `MX_DMA_Init'
C:/ST/STM32CubeIDE_1.15.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/Yassine DEHHANI/Documents/aerosentinel-echo/CM4/Debug/../Core/Src/usart_if.c:108: undefined reference to `MX_USART1_UART_Init'
C:/ST/STM32CubeIDE_1.15.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Core/Src/usart_if.o: in function `vcom_Resume':
C:/Users/Yassine DEHHANI/Documents/aerosentinel-echo/CM4/Debug/../Core/Src/usart_if.c:217: undefined reference to `hdma_usart1_tx'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:68: aerosentinel_echo_CM4.elf] Error 1
"make -j12 all" terminated with exit code 2. Build might be incomplete.
- CM0+:
C:/Users/Yassine DEHHANI/Documents/aerosentinel-echo/Middlewares/Third_Party/LoRaWAN/Mac/LoRaMac.c:1650:40: error: 'McpsIndication_t' {aka 'struct sMcpsIndication'} has no member named 'ResponseTimeout'
1650 | ( MacCtx.McpsIndication.ResponseTimeout > 0 ) )
| ^
make: *** [Middlewares/Third_Party/LoRaWAN/subdir.mk:121: Middlewares/Third_Party/LoRaWAN/LoRaMac.o] Error 1
make: *** Waiting for unfinished jobs....
"make -j12 all" terminated with exit code 2. Build might be incomplete.
Can someone explain to me why is this happening ?