Skip to main content
SL C.1
Associate
April 23, 2026
Question

Sub ghz

  • April 23, 2026
  • 1 reply
  • 60 views

Stm32l010r and s2lp using x cube sub ghz , for custom board just for coding only gpio button status, there are plenty of error, by solving all those 4-5 errors remain and their resolving method is to complete change of middleware files or some code left in file even check through free AI they finally there no such files in middleware add some, for adding it will not compatible with existing file. If tried in stm32wl33cc it also shows so many error but finally there something missing. There are some radio.spi.h and some similar files there in s2lp nucleo example in spirit 2 workshop project, but in s2lp middleware they are not available and look like board specific. If any available example and transmitting and receiving data for s2lp and stm32wl33cc.

1 reply

Technical Moderator
April 23, 2026

Hi SL C.1,

 

I suggest you downloading the STM32WL3x SDK where you can find the basic examples firmware you are looking for.

Here is the link to the website: STM32CubeWL3 | Product - STMicroelectronics

 

BR,
Filippo