The stm32wb5mmg terminal can join the network with the specified panid
1. Requirement description
It is expected that the terminal can join the network with the specified panid
2. Problems encountered during the test
2.1 It was found that the given function ZbStartup cannot enable the terminal to join the network with the specified panid.
2.2 Attempt to use a lower-level function, the network layer function ZbNlmeNetDiscReq, to make a network discovery request. This function returned successfully. In the corresponding callback function, use ZbNwkGetIndex to obtain the network list. This function also returned successfully. However, the network list information has never been obtained (the actual space does have a network). If the network information can be obtained at this stage, the panid can be filtered, but currently, the network information cannot be obtained.
2.3 By using the ZbNlmeJoinReq function of the network layer to join the network, it was found that this function was only declared in the header file zigbee.nwk.h. This function was not defined in the protocol stack, and IAR could not compile successfully. Currently, this function cannot be used.
2.4 If it is implemented to enable the terminal to join the network with the specified panid, are there any other ways?