Skip to main content
SBaro.11
Associate III
March 27, 2025
Question

Trying to reboot STM32WLE5 after flash UART mode

  • March 27, 2025
  • 2 replies
  • 420 views

Hi all,

I've adapted stm32loader python script to working with STM32WL familly, https://github.com/copterust/stm32loader/blob/master/stm32loader.py .

It's working I'm able to flash, read, erase flash. I can flash my firmware. But for now I'd like to reboot my STM after flashing my firmware, but I don't underqtand well if I can do it.

 

I've find some post, but no usefull information, in the python script I have this parameter :

-g address Start executing from address (0x08000000, usually)

But if I try to use it, nothing happend, I have to reset manually ùy STM for reboot.

2 replies

fmm
Associate
April 8, 2025

A response on this topic would be very interesting to me as well! Also by using STM32CubeProgrammer I was not able to directly run the firmware when using UART for flashing.

STTwo-32
Technical Moderator
April 29, 2025

Hello @SBaro.11 

The link you are mentioning is not for an ST Official repository.  So, i could not confirm if it is going to work or not. 

Best Regards.

STTwo-32