Turning BLE on and off in STM32WB55
Hello.
I have problems turning BLE on and off on STM32WB55.
Many examples with BLE start with the lines
MX_APPE_Config();
MX_IPCC_Init();
MX_RF_Init();
MX_APPE_Init();I do the same, and it turns on right away. I don't know how to initialize the sequencer and timeservers by themselves without BLE, so for now, I found a workaround. I turn it off using the RTC timer using the code the esteemed
static void BLE_exit()
{
tBleStatus ret;
if (BleApplicationContext.Device_Connection_Status != APP_BLE_IDLE)
{
ret = aci_gap_terminate(BleApplicationContext.BleApplicationContext_legacy.connectionHandle, 0x13);
if (ret != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG("aci_gap_terminate(), Failed \r\n\r");
}
else
{
APP_DBG_MSG("aci_gap_terminate(), Successfully \r\n\r");
}
}
ret = aci_hal_stack_reset();
if (ret != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG("aci_hal_stack_reset(), Failed \r\n\r");
}
else
{
APP_DBG_MSG("aci_hal_stack_reset(), Successfully \r\n\r");
}
}Then I have buttons on the sequencer tasks, and the time server is still working, and I don't really understand how to enable Bluetooth with a button. Should I somehow reinitialize everything? But how can I not affect the logic of the sequencer and time server? I try to use this function
appe_Tl_Init(); /* Initialize all transport layers */from MX_APPE_Init in the button handler, but nothing happens, and sometimes it even hits the error handler.
Also, maybe there is a more correct way to initialize the sequencer and timeserver without initializing the BLE? How should it be turned on correctly, then?
Also, I wonder how good the idea of using a sequencer and timeserver is for processing the logic of buttons and LEDs? I think that's what it was intended for?
I would be extremely grateful for your help.