Skip to main content
Associate
May 7, 2025
Solved

Upgraded FUS and ble stack not compatible with older firmware codes

  • May 7, 2025
  • 1 reply
  • 619 views

Hi, 

Recently I have mistakenly upgraded to FUS 2.0 and BLE stack 1.22.1 for my stm32wb5mmg chip. I was using FUS 1.2.0 and BLE stack 1.22.0.2 before and the system behaves perfectly fine with the firmware on hand. After upgrading it the device doesn't seem to be advertising and couldn't be detected by any other devices. I have notice that it is impossible to downgrade the FUS version is there a way to tackle the issue? If I wanted to erase the whole chip and copy the memory of a working chip, is that possible?

Best answer by STTwo-32

For now, as you can see on the first warning "With FUS v2.0.0, Coprocessor Binaries can be installed only through the USB interface". This limitation should be fixed on the future.

Best Regards.

STTwo-32 

1 reply

STTwo-32
Technical Moderator
May 7, 2025

Hello @ivan02 

Are you aware of the following notes:

STTwo32_0-1746625470285.png

STM32Cube_FW_WB_V1.22.1/Projects/STM32WB_Copro_Wireless_Binaries/STM32WB5x/Release_Notes.html. Could you please try to connect throw USB, Update FUS and Stack and click on the button "Start Wireless Stack" (you may need to click twice if it generates an issue on the first click). If you still have an issue, Please send me the screenshot of the FUS information (similar to this one):

STTwo32_1-1746625919234.png

Best Regards.

STTwo-32

ivan02Author
Associate
May 7, 2025

Hello @STTwo-32,

 

The board that I am having does not have a usb port configured. Does that means that it is impossible to install the wireless stack?

Best regards,

ivan02

STTwo-32
STTwo-32Best answer
Technical Moderator
May 7, 2025

For now, as you can see on the first warning "With FUS v2.0.0, Coprocessor Binaries can be installed only through the USB interface". This limitation should be fixed on the future.

Best Regards.

STTwo-32