Skip to main content
Emmanuel COMBETTE DE RYMON
ST Employee
July 13, 2021

FAQ : STM32MP1 how to configure Ethernet PHY Clocks

  • July 13, 2021
  • 0 replies
  • 13602 views
During ethernet bring-up with Linux you get the following error : "stm32-dwmac 5800a000.ethernet: Failed to reset the dma"
What does it mean ?
How to configure in Linux and in u-boot the STM32MP1 ethernet clocks for the Ethernet PHY ? 
How to check the clock setting ?
Other issues for bring-up 
https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide
 

1. Symptom

[ 15.650981 ] dwmac4_dma_reset err
[   15.652849] stm32-dwmac 5800a000.ethernet: Failed to reset the dma
[   15.659006] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[   15.668518] stm32-dwmac 5800a000.ethernet eth0: stmmac_open: Hw setup failed
 
Solution   Check Device tree for ethernet clocks (see below) and pin muxing
 

2. Explanation  

Issue is due to the fact PHY does not provide the clock to GMAC, GMAC cannot reset at Ethernet start.


Depending on GMAC interface MII, GMII,RGMII, RMII the clocks are different.

The application note AN5031 §10.1.13 provides ethernet application examples with the different hardware possibilities :

1 RMII with 25MHz with Crystal on PHY, REF_CLK from PHY ->AN5031rv3 figure 44
2 RMII with 25MHz on ETH_CLK  pad from internal RCC (no PHY Crystal), REF_CLK from PHY ->AN5031rv3 figure 44
3 RMII with 50MHz on ETH_CLK  pad (no PHY Crystal), internal REF_CLK from RCC -> AN5031rv3 figure 45
 
4 RGMII with Crystal on PHY, ETH_CLK125 from PHY -> AN5031rv3 figure 46
5 RGMII with 25MHz on ETH_CLK (no PHY Crystal), ETH_CLK125 from PHY -> AN5031rv3 figure 46
6 RGMII with 25MHz Crystal on PHY, internal CLK125 from RCC  -> AN5031rv3 figure 49


For each configuration find the corresponding Linux and u-boot device tree configurations
https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration#DT_configuration
All practical information is explained in this wiki article.

From OpenSTlinux 3.0.1, the properties st,eth_ref_clk_sel or st,eth-ref-clk-sel are deprecated.
They are replaced by  st,ext-phyclk. This property is the same for uboot and kernel.

3. Further background information 
You can see the GMAC clock configuration for the PHY in the RCC reference manual 0436rv5 fig 83 
§ RCC
  Peripheral clock distribution for Ethernet

3 main STM32MP1 pads are to be considered between STM32MP1 GMAC and PHY : 

The ETH_CLK pad which provide a clock to the PHY and
The ETH_REF_CLK pad or ETH_CLK125 pad to get reference clock from the PHY.


Depending on the configuration of your design, you have to configure the device tree,  then the ethernet driver controls the clock configuration via the below registers. 
ETH_CLK_SEL, ETH_REF_CLK_SEL and ETH_SEL are controlled via the register SYSCFG_PMCSETR

ETHMACEN,ETHRXEN,ETHTXEN,ETHCKEN controlled by RCC_MP_AHB6ENSETR
ETHSRC is controlled by RCC_ETHCKSELR 
2.png
Linux device tree properties are define under
https://github.com/STMicroelectronics/linux/blob/v4.19-stm32mp/Documentation/devicetree/bindings/net/stm32-dwmac.txt
Further device tee properties explanations 

  • "eth-ck" : when there is no crystal to feed the PHY, MP1 on Pad ETH_CLK provides the 25 or 50 MHZ clock to PHY  In this case the clode (from ETH_clk fb) is provided by PLL4P or PLL3Q. We are in the AN5031 examples 3 and 6 (above)

3.png

1/ add the clock in DT ethernet node :

clock-names = "stmmaceth","mac-clk-tx","mac-clk-rx","ethstp","syscfg-clk","eth-ck";
clocks = <&rcc ETHMAC>,<&rcc ETHTX>,<&rcc ETHRX>,<&rcc ETHSTP>,<&rcc SYSCFG>,<&rcc ETHCK_K>;
 
<&rcc ETHCK_K>  Enable the 'eth_clk_fb'  Ethernet fig 83 top right corner
4.png

2/ TF-A device tree : ensure in the 'st,pkcs' property contains CLK_ETH_PLL4P or CLK_ETH_PLL3Q have a  enabled 'ck_kern_eth' clock. This changes the bit RCC_ETHCKSELR.ETHSRC
 

3/Ensure the used PLL setting define a 25MHZ or 50MHZ
 

  • "st,eth-clk-sel "(boolean) : set this property in RGMII PHY when PHY does not provide 125Mhz clock to ETH_CLK125  pad

5.png
=>The input ETH_CLK125 pad is not used. The RCC provides 125MHZ clock to GMAC

 

  • "st,eth-ref-clk_sel" (kernel)/st,eth_ref_clk_sel (Uboot) : set this property in RMII mode when ETH_REF_CLK is not provided by PHY case

6.png
=> ETH_RX/REF_CLK pad is not used. Refclock for RMII is from RCC ( eth_clk_fb ) 
Do not set this property in RMII  when the mp1 refclock comes from external PHY via ETH_REF_CLK pad


4. How to check the clock configuration
Dump the state of SYSCFG_PMCSETR
1/enable SYSCFG clk
devmem2 0x50000A10 w 0x10800
2/read SYSCFG_PMCSETR                                                                                                                    
devmem2 0x50020004

Dump the state of RCC_MP_AHB6ENSETR
devmem2 0x
0x5000021C
in uboot md.l  0x5000021C 1
Dump the state of RCC_ETHCKSELR
devmem2 0x
0x500008FC