STM32MP1 how to setup the SDMMC_CK clock frequency in Linux
In the below sdmmc info command, we see timing spec is "mmc DDR52",
whereas clock frequency on SDMMC_CK pin is only at 12.5 MHz
why ?
root@stm32mp151c-oeswa63:~# cat /sys/kernel/debug/mmc0/ios
clock: 25000000 Hz >>>> is SDMMC kernel clock
actual clock: 12500000 Hz >>>> is clock frequency on SDMMC_CK pin chosen by the driver
vdd: 21 (3.3 ~ 3.4 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 3 (8 bits)
timing spec: 8 (mmc DDR52)
signal voltage: 0 (3.30 V)
driver type: 0 (driver type B)
The Linux SDMMC driver decides to takes the highest frequency for the SDMMC_CK pin possible
within the max frequency defined by the SDMMC mode (in device tree binding file and table below)
The frequency on SDMMC_CK pin depends SDMMC kernel clock and SDMMC divider.
This divider is at minimum = 2 when the SDMMC is in DDR mode or 1 when in SDR mode
(RM0436rv5 Figure 693)
PLL4P settings in TF-A device tree :
cfg = < 1 42 20 7 7 PQR(1,0,1) >;
frac = < 0x1800 >;
Let's decode the PLL settings from this two device tree lines,
see https://wiki.st.com/stm32mpu/wiki/Clock_device_tree_configuration_-_Bootloader_specific#Defining_peripheral_PLL_frequencies_with_st-2Cpll_property
HSE=24Mhz
PLL4 freq= HSE/2 * (42+1 + 0x1800/8192) = 12 * 43.75 = 525MHz
20=>DIVP=21 ->525/21=25MHz
0x1800 = 6144
8192 value from RefMan FRACV definition
FracN provide decimal value, between 0 min and almost 1 (8191/8192))
So in current situation, PLL4P is 25MHz.
SDMMC Mode in device Tree : mmc-ddr-3_3v (cf binding and tables below) =>max SDMMC_CK = 52 MHz
Better to set PLL4P=89.57MHz -> SDMMC_CK=44.785
Because if we set 104.5 /2 = 52.25 > 52 MHz so driver will not use div=2.
It will use div=4, 104.5/4 = 26.125 MHz
The list of possible "parent clock" for SDMMC kernel clock
See https://github.com/STMicroelectronics/u-boot/blob/v2020.10-stm32mp/include/dt-bindings/clock/stm32mp1-clksrc.h
The parent clock is selected by the device tree "st,pkcs" property
See https://wiki.st.com/stm32mpu/wiki/Clock_device_tree_configuration_-_Bootloader_specific#Defining_peripheral_kernel_clock_tree_distribution_with_st-2Cpkcs_property
SMMDC mode is set according to the flash device and the expected speed .
All mode are not supported by HW (e.g. HS400 on eMMC)
The driver modes are defined in device tree file:
https://github.com/STMicroelectronics/linux/blob/v5.10-stm32mp/Documentation/devicetree/bindings/mmc/mmc-controller.yaml#L181
SDMMC_CK clock max frequency is in tables of RM0436rv5 "SDMMC operation modes"
It is a maximum, so for example SDMMC in "eMMC High speed DDR" mode can have whatever SDMMC_CK frequency value between 0 and 52MHz.


In RefMan0436 tables present HS200, 200MHz is the max clock is defined here is from the JDEC standard .
On STM32MP1 there is limitation on SDMMC_CK for eMMC and SDCard: Max is not 130MHz but 100MHZ.
I/O max speed is the limitation.
whereas clock frequency on SDMMC_CK pin is only at 12.5 MHz
why ?
root@stm32mp151c-oeswa63:~# cat /sys/kernel/debug/mmc0/ios
clock: 25000000 Hz >>>> is SDMMC kernel clock
actual clock: 12500000 Hz >>>> is clock frequency on SDMMC_CK pin chosen by the driver
vdd: 21 (3.3 ~ 3.4 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 3 (8 bits)
timing spec: 8 (mmc DDR52)
signal voltage: 0 (3.30 V)
driver type: 0 (driver type B)
The Linux SDMMC driver decides to takes the highest frequency for the SDMMC_CK pin possible
within the max frequency defined by the SDMMC mode (in device tree binding file and table below)
The frequency on SDMMC_CK pin depends SDMMC kernel clock and SDMMC divider.
This divider is at minimum = 2 when the SDMMC is in DDR mode or 1 when in SDR mode
(RM0436rv5 Figure 693)
-
Let's take the RCC setup of the command above where:
SDMMC is connected to eMMC in DDR mode " eMMC HighSpeed" (see table below) with SDMMC kernel clock source = PLL4P.
PLL4P settings in TF-A device tree :
cfg = < 1 42 20 7 7 PQR(1,0,1) >;
frac = < 0x1800 >;
Let's decode the PLL settings from this two device tree lines,
see https://wiki.st.com/stm32mpu/wiki/Clock_device_tree_configuration_-_Bootloader_specific#Defining_peripheral_PLL_frequencies_with_st-2Cpll_property
HSE=24Mhz
PLL4 freq= HSE/2 * (42+1 + 0x1800/8192) = 12 * 43.75 = 525MHz
20=>DIVP=21 ->525/21=25MHz
0x1800 = 6144
8192 value from RefMan FRACV definition
FracN provide decimal value, between 0 min and almost 1 (8191/8192))
So in current situation, PLL4P is 25MHz.
The driver sets a DDR mode " eMMC HighSpeed" ("mmc-ddr-3_3v" is in sdmmc device tree node)
and selects the highest clock below 52 MHz freq with div=2. It sets SDMMC_CK to PLL4P/2 =12.5 MHz.
and selects the highest clock below 52 MHz freq with div=2. It sets SDMMC_CK to PLL4P/2 =12.5 MHz.
-
Choice of PLL frequency for the SDMMC kernel clock
SDMMC Mode in device Tree : mmc-ddr-3_3v (cf binding and tables below) =>max SDMMC_CK = 52 MHz
Better to set PLL4P=89.57MHz -> SDMMC_CK=44.785
Because if we set 104.5 /2 = 52.25 > 52 MHz so driver will not use div=2.
It will use div=4, 104.5/4 = 26.125 MHz
The list of possible "parent clock" for SDMMC kernel clock
See https://github.com/STMicroelectronics/u-boot/blob/v2020.10-stm32mp/include/dt-bindings/clock/stm32mp1-clksrc.h
The parent clock is selected by the device tree "st,pkcs" property
See https://wiki.st.com/stm32mpu/wiki/Clock_device_tree_configuration_-_Bootloader_specific#Defining_peripheral_kernel_clock_tree_distribution_with_st-2Cpkcs_property
Background information
SMMDC mode is set according to the flash device and the expected speed .
All mode are not supported by HW (e.g. HS400 on eMMC)
The driver modes are defined in device tree file:
https://github.com/STMicroelectronics/linux/blob/v5.10-stm32mp/Documentation/devicetree/bindings/mmc/mmc-controller.yaml#L181
SDMMC_CK clock max frequency is in tables of RM0436rv5 "SDMMC operation modes"
It is a maximum, so for example SDMMC in "eMMC High speed DDR" mode can have whatever SDMMC_CK frequency value between 0 and 52MHz.


In RefMan0436 tables present HS200, 200MHz is the max clock is defined here is from the JDEC standard .
On STM32MP1 there is limitation on SDMMC_CK for eMMC and SDCard: Max is not 130MHz but 100MHZ.
I/O max speed is the limitation.