BUG: Label or path X_pins_y not found - Compiling the TF-A firmware
I have installed OpenSTLinux SDK + Sources (linux, tf-a, u-boot, optee-os) on a STM32CubeIDE project.
I have compiled optee-os for my custom board, but it did not work so well for tf-a.
This is clearly a bug because I cannot add "i2c2_pin_a" into the .dts file of stm32mp151-stm32-computer-pin-configuration-mx.dts. If I rename
i2c4_pins_mx -> i2c2_pins_amanually inside the .dts file, then the error disapear when I compile. But I cannot do that in STM32CubeIDE because it does not allow me to add "i2c2" for TF-A.
So is there any walk around for this bug?
23:03:35 **** Build of configuration Default for project stm32-computer-pin-configuration_CA7_tf-a-2.8.15-r2 ****
make -f ../Makefile.sdk.ide TF_A_DEVICETREE=stm32mp151a-stm32-computer-pin-configuration-mx TF_A_CONFIG=optee-sdcard stm32 metadata
Wrapper for /opt/st/stm32cubeide_1.16.0/plugins/com.st.stm32cube.ide.mpu.linux.toolchain_2.1.0.202305092038/tools/bin/make
FIP_DEPLOYDIR_ROOT: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../../FIP_artifacts
+ case "$command" in
+ exec make -f ../Makefile.sdk.ide TF_A_DEVICETREE=stm32mp151a-stm32-computer-pin-configuration-mx TF_A_CONFIG=optee-sdcard stm32 metadata
make[1]: Nothing to be done for 'all'.
make[1]: Entering directory '/home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2'
Including bl32/optee/optee.mk
Trusted Firmware-A built for OP-TEE payload support
PSA_FWU_SUPPORT is an experimental feature
CPP /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.dts
DTC /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.dts
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:946.18-29 Label or path fmc_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:947.18-30 Label or path i2c2_pins_a not found
make[1]: Leaving directory '/home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2'
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:948.18-30 Label or path i2c4_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:950.18-34 Label or path qspi_bk1_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:951.18-34 Label or path qspi_bk2_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:952.18-34 Label or path qspi_clk_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:953.18-35 Label or path sdmmc1_b4_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:954.18-36 Label or path sdmmc1_dir_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:955.18-36 Label or path sdmmc1_dir_pins_b not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:956.18-35 Label or path sdmmc2_b4_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:957.18-35 Label or path sdmmc2_b4_pins_b not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:958.18-36 Label or path sdmmc2_d47_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:959.18-36 Label or path sdmmc2_d47_pins_b not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:960.18-36 Label or path sdmmc2_d47_pins_c not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:961.18-36 Label or path sdmmc2_d47_pins_d not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:963.18-31 Label or path uart4_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:964.18-31 Label or path uart4_pins_b not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:965.18-31 Label or path uart7_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:966.18-31 Label or path uart7_pins_b not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:967.18-31 Label or path uart7_pins_c not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:968.18-31 Label or path uart8_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:969.18-32 Label or path usart2_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:970.18-32 Label or path usart2_pins_b not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:971.18-32 Label or path usart2_pins_c not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:972.18-32 Label or path usart3_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:973.18-32 Label or path usart3_pins_b not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:974.18-32 Label or path usart3_pins_c not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:975.18-41 Label or path usbotg_fs_dp_dm_pins_a not found
Error: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.pre.dts:976.18-35 Label or path usbotg_hs_pins_a not found
FATAL ERROR: Syntax error parsing input tree
make[1]: *** [Makefile:1453: /home/lubuntu/Dokument/GitHub/stm32-computer/STM32CubeIDE/stm32-computer-pin-configuration/CA7/tf-a-2.8.15-r2/tf-a-stm32mp-v2.8.15-stm32mp-r2/../build/optee-sdcard-stm32mp15-stm32mp151a-stm32-computer-pin-configuration-mx/fdts/stm32mp151a-stm32-computer-pin-configuration-mx-bl2.dtb] Error 1
make: *** [../Makefile.sdk:232: tf-optee-sdcard-stm32mp15] Error 1
"make -f ../Makefile.sdk.ide TF_A_DEVICETREE=stm32mp151a-stm32-computer-pin-configuration-mx TF_A_CONFIG=optee-sdcard stm32 metadata" terminated with exit code 2. Build might be incomplete.
23:03:37 Build Failed. 31 errors, 0 warnings. (took 1s.745ms)
And the .dts file is:
// SPDX-License-Identifier: (GPL-2.0-or-later OR BSD-3-Clause)
/*
* Copyright (C) 2024, STMicroelectronics - All Rights Reserved
* Author: STM32CubeMX code generation for STMicroelectronics.
*/
/* For more information on Device Tree configuration, please refer to
* https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
*/
/dts-v1/;
#include <dt-bindings/pinctrl/stm32-pinfunc.h>
#include <dt-bindings/clock/stm32mp1-clksrc.h>
#include "stm32mp15-mx.dtsi"
#include "stm32mp151.dtsi"
#include "stm32mp15xa.dtsi"
#include "stm32mp15xxac-pinctrl.dtsi"
#include "stm32mp15-ddr.dtsi"
/* USER CODE BEGIN includes */
/* USER CODE END includes */
/ {
model = "STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mpu-v24.06.26";
compatible = "st,stm32mp151a-stm32-computer-pin-configuration-mx", "st,stm32mp151";
memory@c0000000 {
device_type = "memory";
reg = <0xc0000000 0x20000000>;
/* USER CODE BEGIN memory */
/* USER CODE END memory */
};
/* USER CODE BEGIN root */
/* USER CODE END root */
clocks {
/* USER CODE BEGIN clocks */
/* USER CODE END clocks */
clk_hsi: clk-hsi {
clock-frequency = <64000000>;
/* USER CODE BEGIN clk_hsi */
/* USER CODE END clk_hsi */
};
clk_lse: clk-lse {
clock-frequency = <32768>;
st,drive = < LSEDRV_MEDIUM_HIGH >;
/* USER CODE BEGIN clk_lse */
/* USER CODE END clk_lse */
};
clk_hse: clk-hse {
clock-frequency = <24000000>;
/* USER CODE BEGIN clk_hse */
/* USER CODE END clk_hse */
};
};
}; /*root*/
&pinctrl {
i2c4_pins_mx: i2c4_mx-0 {
pins {
pinmux = <STM32_PINMUX('D', 12, AF4)>, /* I2C4_SCL */
<STM32_PINMUX('D', 13, AF4)>; /* I2C4_SDA */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
sdmmc2_pins_mx: sdmmc2_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
<STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 9, AF10)>, /* SDMMC2_D5 */
<STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
<STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
<STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
<STM32_PINMUX('E', 5, AF9)>, /* SDMMC2_D6 */
<STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('E', 3, AF9)>; /* SDMMC2_CK */
bias-disable;
drive-push-pull;
slew-rate = <3>;
};
};
uart4_pins_mx: uart4_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */
bias-disable;
};
pins2 {
pinmux = <STM32_PINMUX('G', 11, AF6)>; /* UART4_TX */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
};
usb_otg_hs_pins_mx: usb_otg_hs_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 10, ANALOG)>; /* USB_OTG_HS_ID */
};
};
/* USER CODE BEGIN pinctrl */
/* USER CODE END pinctrl */
};
&pinctrl_z {
/* USER CODE BEGIN pinctrl_z */
/* USER CODE END pinctrl_z */
};
&i2c4{
pinctrl-names = "default";
pinctrl-0 = <&i2c4_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2c4 */
/* USER CODE END i2c4 */
};
&rcc{
status = "okay";
/* USER CODE BEGIN rcc */
/* USER CODE END rcc */
st,clksrc=<
CLK_CKPER_DISABLED
CLK_SDMMC12_HCLK6
CLK_STGEN_HSI
CLK_I2C46_PCLK5
CLK_USBO_PLL4R
CLK_UART24_PCLK1
CLK_MPU_PLL1P
CLK_AXI_HSI
CLK_MCU_HSI
>;
st,clkdiv = <
DIV(DIV_MPU, 1)
DIV(DIV_AXI, 0)
DIV(DIV_MCU, 0)
DIV(DIV_APB1, 0)
DIV(DIV_APB2, 0)
DIV(DIV_APB3, 0)
DIV(DIV_APB4, 0)
DIV(DIV_APB5, 0)
DIV(DIV_RTC, 0)
DIV(DIV_MCO1, 0)
DIV(DIV_MCO2, 0)
>;
st,pll_vco {
pll2_vco_800Mhz: pll2-vco-800Mhz {
src=< CLK_PLL12_HSI >;
divmn = < 3 24 >;
};
pll4_vco_480Mhz: pll4-vco-480Mhz {
src=< CLK_PLL4_HSI >;
divmn = < 3 29 >;
};
/* USER CODE BEGIN rcc_st-pll_vco */
/* USER CODE END rcc_st-pll_vco */
};
pll2:st,pll@1 {
compatible = "st,stm32mp1-pll";
reg = <1>;
st,pll = < &pll2_cfg1 >;
pll2_cfg1: pll2_cfg1 {
st,pll_vco = < &pll2_vco_800Mhz >;
st,pll_div_pqr = < 1 1 0 >;
};
/* USER CODE BEGIN pll2 */
/* USER CODE END pll2 */
};
pll4:st,pll@3 {
compatible = "st,stm32mp1-pll";
reg = <3>;
st,pll = < &pll4_cfg1 >;
pll4_cfg1: pll4_cfg1 {
st,pll_vco = < &pll4_vco_480Mhz >;
st,pll_div_pqr = < 3 5 24 >;
};
/* USER CODE BEGIN pll4 */
/* USER CODE END pll4 */
};
};
&sdmmc2{
pinctrl-names = "default";
pinctrl-0 = <&sdmmc2_pins_mx>;
status = "okay";
/* USER CODE BEGIN sdmmc2 */
/* USER CODE END sdmmc2 */
};
&uart4{
pinctrl-names = "default";
pinctrl-0 = <&uart4_pins_mx>;
status = "okay";
/* USER CODE BEGIN uart4 */
/* USER CODE END uart4 */
};
&usbotg_hs{
pinctrl-names = "default";
pinctrl-0 = <&usb_otg_hs_pins_mx>;
status = "okay";
/* USER CODE BEGIN usbotg_hs */
/* USER CODE END usbotg_hs */
};
&usbphyc{
status = "okay";
/* USER CODE BEGIN usbphyc */
/* USER CODE END usbphyc */
};
&usbphyc_port0{
status = "okay";
/* USER CODE BEGIN usbphyc_port0 */
/* USER CODE END usbphyc_port0 */
};
&usbphyc_port1{
status = "okay";
/* USER CODE BEGIN usbphyc_port1 */
/* USER CODE END usbphyc_port1 */
};
/* USER CODE BEGIN addons */
/* USER CODE END addons */