Can't create working FIP binary for Trusted Board Boot
Hi,
we are trying to enable secure boot on a custom board using STM32MP157C.
We are using OpenSTLinux ecosystem v5
- en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
- en.sources-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
What we already did:
- Generated keys using STM32_KeyGen_CLI.exe (publicKeyhash.bin, publicKey.pem, privateKey.pem)
- Write publicKeyhash.bin to OTP using STM32_Programmer_CLI.exe
- Sign the TF-A (BL2) image(.stm32 file) using STM32_SigningTool_CLI.exe
- Verify it worked by getting serial output when booting "NOTICE: Bootrom authentication succeeded"
Next step was embedding certificates in the FIP binary. Until then we built the FIP binary using Makefile.sdk in sources\arm-ostl-linux-gnueabi\tf-a-stm32mp-v2.8.6-stm32mp-r1-r0. If we understand the documentation correctly (https://wiki.st.com/stm32mpu-ecosystem-v5/wiki/TF-A_BL2_Trusted_Board_Boot) generating a FIP with all certificates has to be done using the Makefile in sources\arm-ostl-linux-gnueabi\tf-a-stm32mp-v2.8.6-stm32mp-r1-r0\tf-a-stm32mp-v2.8.6-stm32mp-r1.
So we try to:
- Build binaries with TF-A Makefile.sdk all build target and TRUSTED_BOARD_BOOT=1
- Create fip.bin with certificates by using TF-A Makefile like shown in ecosystem 6 documentation (https://wiki.st.com/stm32mpu/wiki/TF-A_BL2_Trusted_Board_Boot#STM32_MPU_build_options)
The fip binary contains:
Secure Payload BL32 (Trusted OS): offset=0x1000, size=0x2C, cmdline="--tos-fw"
Secure Payload BL32 Extra1 (Trusted OS Extra1): offset=0x2000, size=0x138C0, cmdline="--tos-fw-extra1"
Secure Payload BL32 Extra2 (Trusted OS Extra2): offset=0x16000, size=0x5C000, cmdline="--tos-fw-extra2"
Non-Trusted Firmware BL33: offset=0x72000, size=0xF5D4C, cmdline="--nt-fw"
FW_CONFIG: offset=0x168000, size=0x1EA, cmdline="--fw-config"
HW_CONFIG: offset=0x169000, size=0x13DC8, cmdline="--hw-config"
Trusted key certificate: offset=0x17D000, size=0x284, cmdline="--trusted-key-cert"
Trusted OS Firmware key certificate: offset=0x17E000, size=0x22A, cmdline="--tos-fw-key-cert"
Non-Trusted Firmware key certificate: offset=0x17F000, size=0x22D, cmdline="--nt-fw-key-cert"
Trusted OS Firmware content certificate: offset=0x180000, size=0x2E3, cmdline="--tos-fw-cert"
Non-Trusted Firmware content certificate: offset=0x181000, size=0x254, cmdline="--nt-fw-cert"
STM32MP CONFIG CERT: offset=0x182000, size=0x23F, cmdline="--stm32mp-cfg-cert"When flashing this with STM32CubeProgrammer we get:
11:50:42 : STM32CubeProgrammer API v2.20.0 | Windows-64Bits
11:50:48 : USB speed : High Speed (480MBit/s)
11:50:48 : Manuf. ID : STMicroelectronics
11:50:48 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
11:50:48 : SN : 003F00333231510431333437
11:50:48 : DFU protocol: 1.1
11:50:48 : Board : --
11:50:48 : Device ID : 0x0500
11:50:55 : Read TSV File: C:\Users\gbe\Downloads\dev-image-signed\FlashLayout_emmc_rise_v1_6.tsv
11:50:55 : Number of partitions: 13
11:51:05 : Start Embedded Flashing service
11:51:05 : Opening and parsing file: tf-a-stm32mp157c-rise-usb-signed.stm32
11:51:05 : Memory Programming ...
11:51:05 : File : tf-a-stm32mp157c-rise-usb-signed.stm32
11:51:05 : Size : 212.56 KB
11:51:05 : Partition ID : 0x01
11:51:05 : Download in Progress:
11:51:07 : File download complete
11:51:07 : Time elapsed during download operation: 00:00:01.942
11:51:07 : RUNNING Program ...
11:51:07 : PartID: :0x01
11:51:07 : Start operation done successfully at partition 0x01
11:51:07 : Opening and parsing file: fip-stm32mp157c-rise-optee-signed.bin
11:51:07 : Memory Programming ...
11:51:07 : File : fip-stm32mp157c-rise-optee-signed.bin
11:51:07 : Size : 1.51 MB
11:51:07 : Partition ID : 0x03
11:51:07 : Download in Progress:
11:51:10 : File download complete
11:51:10 : Time elapsed during download operation: 00:00:02.359
11:51:10 : RUNNING Program ...
11:51:10 : PartID: :0x03
11:51:10 : Reconnecting the device ...
11:51:40 : Error: Unable to reconnect the target device: time out expired
11:51:40 : Error: Start operation failed at partition 0x03
11:51:40 : Error: TSV flashing service failed
11:51:41 : Disconnected from device.NOTICE: CPU: STM32MP157F?? Rev.Z
NOTICE: Model: STM32MP157C-Rise Board
NOTICE: Bootrom authentication succeeded
INFO: PMIC version = 0x21
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffdd000
INFO: FCONF: Reading firmware configuration information for: cot_desc
INFO: FCONF: Reading firmware configuration information for: tbbr
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r1.0(debug):v1.1.0-193-gd7fc783c5-dirty(d7fc783c)
NOTICE: BL2: Built : 09:19:19, Oct 30 2025
NOTICE: TRUSTED_BOARD_BOOT support enabled
INFO: Using crypto library 'stm32_crypto_lib'
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: phase ID :3, Manifestation 3 at c7183000
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 1
INFO: Loading image id=17 at address 0x2ffff000
INFO: Image id=17 loaded: 0x2ffff000 - 0x2ffff23e
ERROR: BL2: Failed to load image id 1 (-80)
It looks like STM32MP CONFIG CERT (id 17) is successfully loaded but then it fails to load FW_CONFIG (id 1).
Any help would be appreciated!