Skip to main content
Associate
July 15, 2025
Question

Can't open /dev/ttyRPMSG0

  • July 15, 2025
  • 2 replies
  • 260 views

I used the same code. Previously, I was using STM32Cube_FW_MP1_V1.2.0, but after forcibly upgrading to STM32Cube_FW_MP1_V1.7.0 using CubeIDE, the compiled firmware can no longer generate a virtual serial port( /dev/ttyRPMSG0).

 

This is the log I used with version 1.7.

[ 3276.128100] remoteproc remoteproc0: powering up m4
[ 3276.141973] remoteproc remoteproc0: Booting fw image RPMsg_UART_CM4_te.elf, size 2549508
[ 3276.149267] mlahb:m4@10000000#vdev0buffer: assigned reserved memory node vdev0buffer@10042000
[ 3276.164561] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 3276.168677] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty addr 0x400
[ 3276.188640] mlahb:m4@10000000#vdev0buffer: registered virtio0 (type 7)
[ 3276.203388] remoteproc remoteproc0: remote processor m4 is now up

 

This is the log I used with version 1.2

[ 3395.909607] remoteproc remoteproc0: powering up m4
[ 3395.954530] remoteproc remoteproc0: Booting fw image RPMsg_UART_CM4.elf, size 2042304
[ 3395.961362] mlahb:m4@10000000#vdev0buffer: assigned reserved memory node vdev0buffer@10042000
[ 3395.975942] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 3395.980062] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x0
[ 3395.994741] mlahb:m4@10000000#vdev0buffer: registered virtio0 (type 7)
[ 3395.999912] remoteproc remoteproc0: remote processor m4 is now up
[ 3396.028384] rpmsg_tty virtio0.rpmsg-tty-channel.-1.0: new channel: 0x400 -> 0x0 : ttyRPMSG0


This is a portion of my code, generated by CubeIDE. 

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 if(IS_ENGINEERING_BOOT_MODE())
 {
 /* Configure the system clock */
 SystemClock_Config();
 }
 else
 {
 /* IPCC initialisation */
 MX_IPCC_Init();
 /* OpenAmp initialisation ---------------------------------*/
 MX_OPENAMP_Init(RPMSG_REMOTE, NULL);
 }

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 /* USER CODE BEGIN 2 */

 if (VIRT_UART_Init(&huart0) != VIRT_UART_OK)
 {

	 Error_Handler();
 }

 if(VIRT_UART_RegisterCallback(&huart0, VIRT_UART_RXCPLT_CB_ID, VIRT_UART0_RxCpltCallback) != VIRT_UART_OK)
 {
	 Error_Handler();
 }
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */

 

2 replies

Olivier GALLIEN
Technical Moderator
July 18, 2025

Hi @Tom18 

 

Going from 1.2 to 1.7 is a huge jump. Did you also move to latest CubeIDE ? 

 

Olivier 

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tom18Author
Associate
July 21, 2025

Yes, I'm using the latest version of cubeIDE v1.90, but it doesn't work. My device is mp151. I created a new demo to test it, but it still didn't work. Ultimately, I could only choose not to upgrade the firmware library

ST Employee
July 25, 2025

Hi @Tom18 ,

You can take reference from the application which is present on this location:
STM32Cube_FW_MP1_V1.7.0\Projects\STM32MP157C-DK2\Applications\OpenAMP\OpenAMP_TTY_echo
On running the project present of this location, I got these logs.

shivam203_0-1753439538899.png

Thank you

                                                                                                                                                                                           
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.