Cannot start to count up TIM3 in PWM generation mode
I use STM32MP151CAA3 mounted on my own board.
I want to start to count up TIM3 in PWM generation mode in Cortex-M4.
I have written following code, However, TIM3 doesn't start to count up (After Line 56, TIM3_CNT value doesn't change at all).
In this code, PB04 port is used as PWM output port.
void TIM3_Count_Start(void)
{
TIM_HandleTypeDef m_handleTim3;
TIM_OC_InitTypeDef sConfigOC;
TIM_SlaveConfigTypeDef sSlaveConfig;
TIM_MasterConfigTypeDef sMasterConfig;
GPIO_InitTypeDef GPIO_InitStruct;
/* Peripheral clock enable */
__TIM3_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
GPIO_InitStruct.Alternate = GPIO_AF2_TIM3;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
m_handleTim3.Instance = TIM3;
m_handleTim3.Init.Prescaler = 0;
m_handleTim3.Init.CounterMode = TIM_COUNTERMODE_UP;
m_handleTim3.Init.Period = 0;
m_handleTim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
HAL_TIM_Base_Init(&m_handleTim3);
HAL_TIM_PWM_Init(&m_handleTim3);
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0xFFFF;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
HAL_TIM_PWM_ConfigChannel(&m_handleTim3, &sConfigOC, TIM_CHANNEL_1);
sSlaveConfig.SlaveMode = TIM_SLAVEMODE_EXTERNAL1;
sSlaveConfig.InputTrigger = TIM_TS_ITR0;
HAL_TIM_SlaveConfigSynchronization(&m_handleTim3, &sSlaveConfig);
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
HAL_TIMEx_MasterConfigSynchronization(&m_handleTim3, &sMasterConfig);
TIM3->PSC = 399;
TIM3->ARR = 49;
TIM3->CCR1 = 0xFFFF;
TIM3->CR1 |= 0x0080;
TIM3->EGR |= TIM_EGR_UG;
TIM3->CCER |= 0x0001;
TIM3->SR = 0;
TIM3->DIER |= 0x0001;
TIM3->CR1 |= 0x0001; /* TIM3 Count Start */
}Is there any missing in above code?
Best Regards.
H. Masuda