Disable weston autostart in STM32MP157C-DV2
I am evaluate the STM32MP157C-DV2 board.
I tried to disable the automatic start of the weston service by referring to the wiki below.
https://wiki.st.com/stm32mpu/wiki/How_to_stop_and_start_Weston
root@stm32mp1:~# systemctl disable weston@root.service
root@stm32mp1:~# reboot
but it does not work properly.
Still the weston service will run automatically and a demo application will appear.
Status is static after disable as shown below.
root@stm32mp1:~# systemctl disable weston@root.service
root@stm32mp1:~# systemctl status weston@root.service
[[0;1;32m*[[0m weston@root.service - Weston Wayland Compositor (on tty7)
Loaded: loaded (/lib/systemd/system/weston@.service; static; vendor preset: disabled)
Active: [[0;1;32mactive (running)[[0m since Fri 2021-03-05 06:00:23 UTC; 16min ago
Main PID: 3884 (weston)
Memory: 792.0K
CGroup: /system.slice/system-weston.slice/weston@root.service
> 3884 /usr/bin/weston --log=/var/log/weston.log --xwayland
What's the problem?
Thank you in advance.