Driver stm32_tamp_nvram on node nvram@46010100 failed
I having some issues with nvram in op-tee.
I don't know what this happen. It seems that op-tee want to say to me that 0xffff0006 is TEE_ERROR_BAD_PARAMETERS. In this case, I don't use any tamper and don't have LSE.
I think this is a bug because my ST TF-A and ST Op-tee assumes that LSE must be available to proceed. I made a specific hack in ST TF-A that avoids the LSE configuration to continue working. When ST TF-A was starting. It was going to enable clock ID 5, which is LSE, no matter if I have LSE disabled or enable. An if-statement solved this issue.
Do you have any clue what's can be the cause of this?
Processor: STM32MP257FAK
F/TC:0 0 process_probe_list:657 Probe loop 6 after 4 for deferral(s)
D/TC:0 0 print_probe_list:504 Probe list: 3 elements
D/TC:0 0 print_probe_list:506 |- Driver stm32-gpu probes on node gpu@48280000
D/TC:0 0 print_probe_list:506 |- Driver stm32-tamp probes on node tamp@46010000
D/TC:0 0 print_probe_list:506 |- Driver stm32-cpu probes on node cpu@0
D/TC:0 0 print_probe_list:510 `- Probe list end
D/TC:0 0 print_probe_list:516 Failed list: 0 elements
D/TC:0 0 print_probe_list:521 `- Failed list end
F/TC:0 0 probe_driver_node:543 Probing stm32-cpu on node cpu@0
D/TC:0 0 probe_driver_node:556 element: stm32-cpu on node cpu@0 deferred 1 time(s)
F/TC:0 0 probe_driver_node:543 Probing stm32-tamp on node tamp@46010000
D/TC:0 0 gic_it_set_cpu_mask:410 cpu_mask: writing 0x3ff0000 to 0x72a1082c
D/TC:0 0 gic_it_set_cpu_mask:412 cpu_mask: 0x3030000
D/TC:0 0 gic_it_set_prio:426 prio: writing 0x1 to 0x72a1042e
D/TC:0 0 stm32_tamp_parse_passive_conf:1649 Passive conf from dt: precharge=0, nb_sample=0, clk_div=32768
D/TC:0 0 stm32_tamp_parse_active_conf:1874 Active conf from dt: no filter clk_div=1
F/TC:0 0 stm32_tamp_probe:2057 STM32 TAMPER V3.4
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:636 Backup registers mapping :
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:637 ********START of zone 1********
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:638 Protection Zone 1-RIF1 begins at register: 0
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:639 Protection Zone 1-RIF2 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:641 Protection Zone 1-RIF2 ends at register: 127
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:643 ********END of zone 1********
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:644 ********START of zone 2********
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:645 Protection Zone 2-RIF1 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:647 Protection Zone 2-RIF2 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:649 Protection Zone 2-RIF2 ends at register: 0
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:652 ********END of zone 2********
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:653 ********START of zone 3********
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:654 Protection Zone 3-RIF1 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:656 Protection Zone 3-RIF0 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:658 Protection Zone 3-RIF2 begins at register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:660 Protection Zone 3-RIF2 ends at the last register: 128
D/TC:0 0 stm32_tamp_apply_bkpr_rif_conf:661 ********END of zone 3********
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP1 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP2 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP3 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP4 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP5 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP6 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP7 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP8 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP9 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP10 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP11 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP12 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP14 disabled
F/TC:0 0 stm32_tamp_set_int_config:790 INT_TAMP15 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP1 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP2 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP3 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP4 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP5 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP6 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP7 disabled
F/TC:0 0 stm32_tamp_set_ext_config:840 EXT_TAMP8 disabled
F/TC:0 0 stm32_tamp_set_config:1163 Set passive conf 00000080
F/TC:0 0 stm32_tamp_set_config:1168 Set active conf1 00000000
F/TC:0 0 stm32_tamp_set_config:1172 Set active conf2 00000000
D/TC:0 0 add_node_to_probe:748 element: stm32_tamp_nvram on node nvram@46010100
D/TC:0 0 print_probe_list:504 Probe list: 3 elements
D/TC:0 0 print_probe_list:506 |- Driver stm32-gpu probes on node gpu@48280000
D/TC:0 0 print_probe_list:506 |- Driver stm32-cpu probes on node cpu@0
D/TC:0 0 print_probe_list:506 |- Driver stm32_tamp_nvram probes on node nvram@46010100
D/TC:0 0 print_probe_list:510 `- Probe list end
D/TC:0 0 print_probe_list:516 Failed list: 0 elements
D/TC:0 0 print_probe_list:521 `- Failed list end
D/TC:0 0 probe_driver_node:550 element: stm32-tamp on node tamp@46010000 initialized
F/TC:0 0 probe_driver_node:543 Probing stm32-gpu on node gpu@48280000
D/TC:0 0 probe_driver_node:556 element: stm32-gpu on node gpu@48280000 deferred 4 time(s)
F/TC:0 0 process_probe_list:657 Probe loop 7 after 5 for deferral(s)
D/TC:0 0 print_probe_list:504 Probe list: 3 elements
D/TC:0 0 print_probe_list:506 |- Driver stm32-cpu probes on node cpu@0
D/TC:0 0 print_probe_list:506 |- Driver stm32_tamp_nvram probes on node nvram@46010100
D/TC:0 0 print_probe_list:506 |- Driver stm32-gpu probes on node gpu@48280000
D/TC:0 0 print_probe_list:510 `- Probe list end
D/TC:0 0 print_probe_list:516 Failed list: 0 elements
D/TC:0 0 print_probe_list:521 `- Failed list end
F/TC:0 0 probe_driver_node:543 Probing stm32-gpu on node gpu@48280000
D/TC:0 0 probe_driver_node:556 element: stm32-gpu on node gpu@48280000 deferred 5 time(s)
F/TC:0 0 probe_driver_node:543 Probing stm32_tamp_nvram on node nvram@46010100
E/TC:0 0 probe_driver_node:565 Failed to probe stm32_tamp_nvram on node nvram@46010100: 0xffff0006
F/TC:0 0 probe_driver_node:543 Probing stm32-cpu on node cpu@0
D/TC:0 0 probe_driver_node:556 element: stm32-cpu on node cpu@0 deferred 2 time(s)
D/TC:0 0 process_probe_list:697 Unresolved dependencies after 7 rounds, 6 deferred
E/TC:0 0 probe_dt_drivers:902 Probe sequence result: 0x80000000
D/TC:0 0 print_probe_list:504 Probe list: 2 elements
D/TC:0 0 print_probe_list:506 |- Driver stm32-gpu probes on node gpu@48280000
D/TC:0 0 print_probe_list:506 |- Driver stm32-cpu probes on node cpu@0
D/TC:0 0 print_probe_list:510 `- Probe list end
D/TC:0 0 print_probe_list:516 Failed list: 1 elements
E/TC:0 0 print_probe_list:518 |- Driver stm32_tamp_nvram on node nvram@46010100 failed
D/TC:0 0 print_probe_list:521 `- Failed list end
E/TC:0 0 Panic at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r2/core/kernel/dt_driver.c:904 <probe_dt_drivers>
E/TC:0 0 TEE load address @ 0x82000000
E/TC:0 0 Call stack:
E/TC:0 0 0x82008140
E/TC:0 0 0x82046c74
E/TC:0 0 0x82042ca0
E/TC:0 0 0x82048980
E/TC:0 0 0x82007bac
E/TC:0 0 0x82007f44