Question
Ethernet Ping issue in UbootV2022.10
- November 25, 2023
- 0 replies
- 2003 views
Hello,
We are using STM32157AAA3 Processor in our custom board and Microchip Ksz9893 switch for ethernet and the switch is configured using i2c.
- when we are trying to ping ethernet in RGMII mode in U-Boot v2022.10-stm32mp-r1 we are getting the Rx-clock frequency 125MHz but the Tx clock is configuring for 2.5Mhz and we are getting ping is not alive.
- when we try to ping ethernet in RMII Mode with auto negotiation it works fine.
- And we are able to ping ethernet in linux(v5.13) with fixed-link property in rgmii and rmii but when we are trying to use fixed-link in ubootV2022.10 we are getting cpu reset issue.
Please find the below attached screen shots for our processor specific and board specific configurations and output log
- with out fixed-link we are getting
without fixed-link property
- with fixed-link we are getting
With fixed-link property
please help us in this regards.
regards,
Srikanth.