FileExistsError when enabling i2cdetect on custom-image Yocto
I have been following a series of tutorials on Yocto and STM32MP1 by Digikey.
I do have a question I am hoping you can give me some pointers on, while building the custom image after activating the i2cdetect, i get the following error
ERROR: busybox-1.31.1-r0 do_package: Error executing a python function in exec_func_python() autogenerated:
The stack trace of python calls that resulted in this exception/failure was:
File: 'exec_func_python() autogenerated', lineno: 2, function: <module>
0001:
*** 0002:ptest_update_alternatives(d)
0003:
File: '/home/raymond/Projects/yocto/poky/meta/classes/ptest.bbclass', lineno: 98, function: ptest_update_alternatives
0094: for alt_name, alt_link, alt_target, _ in alternatives:
0095: # Some alternatives are for man pages,
0096: # check if the alternative is in PATH
0097: if os.path.dirname(alt_link) in bin_paths:
*** 0098: os.symlink(alt_target, os.path.join(ptest_bindir, alt_name))
0099:}
0100:
0101:do_configure_ptest_base[dirs] = "${B}"
0102:do_compile_ptest_base[dirs] = "${B}"
Exception: FileExistsError: [Errno 17] File exists: '/bin/busybox.suid' -> '/home/raymond/Projects/yocto/build-mp1/tmp/work/cortexa7t2hf-neon-vfpv4-poky-linux-gnueabi/busybox/1.31.1-r0/package/usr/lib/busybox/ptest/bin/i2cdetect'
ERROR: Logfile of failure stored in: /home/raymond/Projects/yocto/build-mp1/tmp/work/cortexa7t2hf-neon-vfpv4-poky-linux-gnueabi/busybox/1.31.1-r0/temp/log.do_package.16030
ERROR: Task (/home/raymond/Projects/yocto/poky/meta/recipes-core/busybox/busybox_1.31.1.bb:do_package) failed with exit code '1'
I have tried
What maybe the cause for this?