Skip to main content
Associate III
March 6, 2026
Question

Getting started with X-LINUX-GNSS1 needs to be updated.

  • March 6, 2026
  • 1 reply
  • 117 views

Section 5.1.1 Step 3 says that 

Copy the dts file from the directory: x-linux-gnss1-app\linux-kernel\patch\5.15\kernel to the kernel
source directory at <KERNEL SOURCE PATH>/ arch/arm/boot/dts/

But in the latest X-LINUX-GNSS1 package, the linux kernel is 6.1.11 and there are 3 patch files and 1 fragment file is present. 

It is unclear what to copy exactly. 

@Saurabh.Rawat 

1 reply

Saurabh.Rawat
ST Employee
April 6, 2026

Hello @embeddedbro  , 

The Device tree and kernel patches are provided in the 6.1 directory. You can apply them.

Regards,

S