How can i solve iso-codes-4.4-r0 do fetch error?(I proceeded according to the procedures of the WIKI Page. : https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package)
- July 7, 2020
- 1 reply
- 2707 views
Hello guys.
I am proceeding in the manner provided on the WIKI page(https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package).
However, the following problems still occur in Step 6.
[error codes]
-----------------------------------------------------------------------------------------------------------------------
WARNING: iso-codes-4.4-r0 do_fetch: Failed to fetch URL git://salsa.debian.org/iso-codes-team/iso-codes.git;protocol=http, attempting MIRRORS if available
ERROR: iso-codes-4.4-r0 do_fetch: Fetcher failure: Unable to find revision 38edb926592954b87eb527124da0ec68d2a748f3 in branch master even from upstream
ERROR: iso-codes-4.4-r0 do_fetch: Fetcher failure for URL: 'git://salsa.debian.org/iso-codes-team/iso-codes.git;protocol=http'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/parksh/STM32MPU_EV1_Workspace/SDK/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/all-ostl-linux/iso-codes/4.4-r0/temp/log.do_fetch.39779
ERROR: Task (/home/parksh/STM32MPU_EV1_Workspace/SDK/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-06-24/layers/openembedded-core/meta/recipes-support/iso-codes/iso-codes_4.4.bb:do_fetch) failed with exit code '1'
-----------------------------------------------------------------------------------------------------------------------
I think there is a problem with that brench(do_fetch).
(I don't see the corresponding brench on the iso-codes page.)
How do I solve this problem?
The contents of log_do_fetch are uploaded as attachments.
thanks