Question
How to build a minimal OpenSTLinux SD image with all drivers/hardware support for the DK2 Discovery board ?
I am confused by the different packages ,Starter, Distribution and Developer.
Which one do I need to install/setup/build to have as the end result a "minimal" cli/shell based SD card image with support for all hardware on the DK2 board ? a "clean" rootfs with no examples, no Wayland/X11 .. just command line and all drivers for the board installed ?