How to configure GPIO on STM32MP157A-DK1 board?
Hello everyone, I use the STM32MP157A-DK1 on my project but I have a problem
1- In the CubeMX, when you want to use a GPIO in output or input, why can not we select the context (cortex A7 or cortex M4)?

2- When you set a GPIO as an output or input to CubeMX and generate code for SW4STM32, the GPIO you defined is not automatically configured in main.c, can I know why? please

3- In SW4ST32 (main.c), when you manually set a GPIO and try to flash LEDs that you connect to the PG3 for example, no signal arrives on the PORT, did I make a mistake?


BEST REGARDS