Hi @FFont.1
The gatttool is available after installing the package bluez5-noinst-tools :
root@stm32mp1:~# apt-get install bluez5-noinst-tools
Reading package lists... Done
Building dependency tree
Reading state information... Done
The following NEW packages will be installed:
bluez5-noinst-tools
0 upgraded, 1 newly installed, 0 to remove and 0 not upgraded.
...
root@stm32mp1:~# which gatttool
/usr/bin/gatttool
root@stm32mp1:~# gatttool -h
Usage:
gatttool [OPTION?]
Help Options:
-h, --help Show help options
--help-all Show all help options
--help-gatt Show all GATT commands
--help-params Show all Primary Services/Characteristics arguments
--help-char-read-write Show all Characteristics Value/Descriptor Read/Write arguments
Application Options:
-i, --adapter=hciX Specify local adapter interface
-b, --device=MAC Specify remote Bluetooth address
-t, --addr-type=[public | random] Set LE address type. Default: public
-m, --mtu=MTU Specify the MTU size
-p, --psm=PSM Specify the PSM for GATT/ATT over BR/EDR
-l, --sec-level=[low | medium | high] Set security level. Default: low
-I, --interactive Use interactive mode
Best regards
JM