How to set VSW domain for "stm32mp151c" custom board as openstlinux dts (for using RETRAM)
Hi All.
I want to use the battery to power the RETRAM so that the contents of the RETRAM can be preserved even if the board is not powered.
To do this, I connected the battery to the VBAT pin and set the "PWR_CR2_RREN" value to the "PWR_CR2" register of the M4 core firmware.
However, when booting from Linux, the value set in the "PWR_CR2" register disappears.
When booting in "Engineering Mode" and running only with the firmware of the M4 core, the setting value of the "PWR_CR2" register does not disappear even when the main power is turned off.
Is there anything I need to add when I create the "dts" file to enable that feature?
Please give me a lot of advice.
Thanks
Regards
Machilus