Skip to main content
Visitor II
July 16, 2025
Question

IMX219 + STM32MP257F-DK: DCMIPP Streaming Fails with Error -22

  • July 16, 2025
  • 2 replies
  • 389 views

 

Hello ST Community,

I'm using the STM32MP257F-DK board with the Waveshare IMX219 camera (connected via MIPI CSI2).

I've configured the device tree for the sensor, and the camera appears correctly under /dev/v4l-subdev7. I’m trying to capture raw video using:

 

 
v4l2-ctl -d /dev/video0 --stream-mmap --stream-count=10 --stream-to=out.raw

But I get the following error:

 

 
[ dcmipp 48030000.dcmipp: failed to start streaming (-22) ]
VIDIOC_STREAMON returned -1 (Invalid argument)

What’s Working:

  • Device tree loads fine

  • IMX219 is detected

  • Sensor controls are visible via v4l2-ctl -L

What’s Not Working:

  • Streaming fails with error -22 from DCMIPP

What I Need Help With:

  • What could cause this Invalid argument during streaming?

  • Is there any resolution/format restriction for DCMIPP?

  • Any working example for IMX219 + STM32MP25 + DCMIPP would help a lot

Thanks in advance!

2 replies

Erwan SZYMANSKI
Technical Moderator
July 16, 2025

Hello @Dhanu_bhosale ,
Did you follow this wiki page for DCMIPP configuration ? https://wiki.st.com/stm32mpu/wiki/STM32MP2_V4L2_camera_overview#Grab_a_frame_from_a_RAW_sensor--with_ISP_demosaicing

Can you share your own configuration regarding your sensor (I am not familiar with this particular camera) ?

The possible root cause could be a wrong alignment between element of the complete pipe (Cam + CSI + DCMIPP subdevs) in term of size / pixel format. You can check the complete configuration applied thanks to this command here: https://wiki.st.com/stm32mpu/wiki/STM32MP2_V4L2_camera_overview#Get_the_topology_of_the_camera_subsystem

Launch this command after your overall configuration, and check the complete path with format negotiated and so  on. Do not hesitate to share these inputs if you are still blocked.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
August 8, 2025

Hi Dhanu , 
                 Can you share the device tree for my reference .

Thanks & Regards 
Mayur Dongre