Skip to main content
iheb
Associate III
July 12, 2022
Solved

Is it possible to program STM32MP1 using UART?

  • July 12, 2022
  • 1 reply
  • 1526 views

I was wondering if its possible to directly flash the STM32MP1 using UART using the STM32CubeProgrammer ?

if so are there any tutorials that can be followed ?

This topic has been closed for replies.
Best answer by PatrickF

Hi,

Please see this page: https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Using_STM32Programmer_over_UART

Note that programming complete Linux image using UART will be very (very!) long (starter package = ~700MBytes , estimated to ~18 hours). It is recommended for tests purposes and reserved to flash up to uBoot.

It is recommended to use USB.

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

1 reply

PatrickF
PatrickFBest answer
Technical Moderator
July 12, 2022

Hi,

Please see this page: https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Using_STM32Programmer_over_UART

Note that programming complete Linux image using UART will be very (very!) long (starter package = ~700MBytes , estimated to ~18 hours). It is recommended for tests purposes and reserved to flash up to uBoot.

It is recommended to use USB.

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here