Skip to main content
Lead
September 10, 2024
Question

Is there any alternative Linux OS for the STM32MP1 system?

  • September 10, 2024
  • 1 reply
  • 994 views

Hi!

I'm looking for an alternative Linux OS for the STM32MP1 system. I'm currently using OpenSTLinux, but it's very buggy and have a lack of lots of packages.

Can you recommend a Linux OS or that works with 512 MB Ram + 650 MHz CPU?

I'm planning to only replace the rootfs folder with the new linux distro.

1 reply

Macdog
Associate III
September 17, 2024

Several years back we ended up creating a Buildroot distribution, since then I believe that STMicro has offered official buildroot distributions for their ecosystem.    What packages are you looking for that are not available using Yocto or Buildroot?

 

DMårtAuthor
Lead
September 17, 2024

@Macdog 

I have created a Linux distro for stm32mp1 by using buiodroot.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-ComputerSTM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer