Associate III
June 16, 2025
Question
Issue Compiling U-boot for STM32MP25 using Developer Package + X-LINUX-RT expansion package
- June 16, 2025
- 0 replies
- 293 views
Hello,
I'm trying compiling OpenSTLinux 6.6 for STM32MP257-EV1 using developer package + X-LINUX-RT expansion package. I've followed X-LINUX-RT expansion package guide at par. 7.2 and compiled linux kernel and optee successfully.
Now I'm trying to compile u-boot but the process stops with following errors:
LD u-boot
OBJCOPY u-boot.srec
OBJCOPY u-boot-nodtb.bin
RELOC u-boot-nodtb.bin
make[4]: *** No rule to make target 'arch/arm/dts/stm32mp257f-ev1-rt.dtb', needed by 'dtbs'. Stop.
make[3]: *** [/home/marco/MP257_Ecosystem6/en.SOURCES-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06_X-LINUX-RT/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/aarch64-ostl-linux/u-boot-stm32mp-v2023.10-stm32mp-r1-r0/u-boot-stm32mp-v2023.10-stm32mp-r1/dts/Makefile:44: arch-dtbs] Error 2
make[2]: *** [/home/marco/MP257_Ecosystem6/en.SOURCES-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06_X-LINUX-RT/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/aarch64-ostl-linux/u-boot-stm32mp-v2023.10-stm32mp-r1-r0/u-boot-stm32mp-v2023.10-stm32mp-r1/Makefile:1162: dts/dt.dtb] Error 2
make[2]: Leaving directory '/home/marco/MP257_Ecosystem6/MP2_X-LINUX-RT_build/u-boot-v2023.10/stm32mp25_defconfig'
make[1]: *** [Makefile:177: sub-make] Error 2
make[1]: Leaving directory '/home/marco/MP257_Ecosystem6/en.SOURCES-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06_X-LINUX-RT/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/aarch64-ostl-linux/u-boot-stm32mp-v2023.10-stm32mp-r1-r0/u-boot-stm32mp-v2023.10-stm32mp-r1'
make: *** [/home/marco/MP257_Ecosystem6/en.SOURCES-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06_X-LINUX-RT/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/aarch64-ostl-linux/u-boot-stm32mp-v2023.10-stm32mp-r1-r0/u-boot-stm32mp-v2023.10-stm32mp-r1/../Makefile.sdk:175: uboot-stm32mp25_defconfig] Error 1This is the command I used:
make -f $PWD/../Makefile.sdk -j12 BLD_PATH=$BLD_PATH_UBOOT UBOOT_CONFIG="default" UBOOT_DEFCONFIG="stm32mp25_defconfig" UBOOT_BINARY=u-boot.dtb DEPLOYDIR="${FIP_DEPLOYDIR_ROOT}/u-boot" DEVICE_TREE=stm32mp257f-ev1-rt ubootIt's taken from one suggested in the guide (par. 7.2.4.2 in u-boot section for stm32mp257f-ev1-rt.dts) I only added the param BLD_PATH=$BLD_PATH_UBOOT to compile outside source code tree.
I attached the complete compile log if needed.
Can someone help me, please
Regards
Marco.