Skip to main content
RBruè.1
Associate II
July 29, 2021
Solved

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,6)

  • July 29, 2021
  • 2 replies
  • 1340 views

Hi, I've created a SD card following this guide. The generated SD card partitions can be seen in the screenshot here below. It seems to boot correctly until the kernel prompts the following error:

[ 4.200445] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,6) ]---

How to solve this?

Thank you.

0693W00000D0wxrQAB.png

This topic has been closed for replies.
Best answer by RBruè.1

I've re-written the SD card another time, and now it works as expected, don't sure why it wasn't working before.

2 replies

RBruè.1
RBruè.1AuthorBest answer
Associate II
July 29, 2021

I've re-written the SD card another time, and now it works as expected, don't sure why it wasn't working before.

Olivier GALLIEN
Technical Moderator
July 29, 2021

Hi @Riccardo Bruè​ ,

I will check at my end if there's no problem with the scripts itself.

May you have possibility to program the SDCard on board with STM32CubeProg ?

But this can also come from a wrong uboot configuration.

You have compiled all material with Distri pack right ?

Olivier

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.