Kernel Version for OpenSTLinux on STM32MP25 Series
Hi,
I was wondering if there's any guidance on the approximate timeline for rebasing OpenSTLinux from kernel 6.6 to kernel 6.12 (autumn 2024) or to kernel 6.15, 6.16, 6.17 or 6.18?
I know that this is an enormous amount of work and a very complex task - the STM32MP25 is an extremely advanced chip and there are some significant changes in the kernel between kernel 6.6 and kernel 6.12 LTS and later kernels so it won't be possible to give any definite timescales for this at this stage.
It would be great to have a very approximate rough idea of the planned timelines for this since the advances in the kernel between 6.6 and 6.15 LTS make significant improvements in the kernel's ability to handle advanced functionality on the STM32MP25 and on ST image sensors. :)
Thank you very much for your help!
Will