Skip to main content
Associate II
November 4, 2024
Question

PHYTEC STM32MP135 LCD PANEL DTS

  • November 4, 2024
  • 1 reply
  • 1207 views

Hello everyone,

I am using the STM32MP135 SoM from PHYTEC, and I’m creating a custom device tree source (DTS) file tailored to our carrier board. I’m having trouble controlling the backlight PWM signal. I’m unable to enable the PWM and enable signal as expected, although I can change the enable pin status if I remove the enable pin definition from the backlight node. Additionally, there is no [used] indication next to GPIOI pin 0, which I’ve configured as the panel enable GPIO. I suspect this issue may be related to the LCD node configuration.

I’ve attached my GPIO states and the DTS file for reference.

image_2024-11-05_005132081.png

image_2024-11-05_005307530.png

image_2024-11-05_005326551.png

 

1 reply

Olivier GALLIEN
Technical Moderator
November 7, 2024

Hi @batuhanky 

Did you try to get support from PHYTEC ? 

Thanks

Olivier 

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
November 7, 2024

Perhaps indicate how it would work in the generic non-board specific sense, and if the DTS file misses specific details or is otherwise internally inconsistent. 

That would be more helpful than entirely punting and might have broader impact. 

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..