Skip to main content
Associate III
December 9, 2025
Question

Regarding M33 on stm32mp257

  • December 9, 2025
  • 1 reply
  • 328 views

Hello

 

We are implementing the memory CRC generation sequence as described in the reference manual. According to the documented procedure, the following steps must be executed:

1. Write 0x0 in CRCC[1:0] of RAMCFG_xCCR1 to deactivate the CRC.
2. Write 1 in SRAMHWERDIS of RAMCFG_xCR to disable the hardware erase.
3. Select the buffer size to take into account during the CRC computation by setting
CRCBS[2:0] in RAMCFG_xCCR1.
4. Write 0x1 in CRCC[1:0] of RAMCFG_xCCR1 to activate the CRC.
5. Write 1 in CRCCS of RAMCFG_xCCR2 to start the CRC computation.
The calculated signature is stored in RAMCFG_xCCSR when CRCEOC is set
in RAMCFG_xCSR.

While following this sequence, the CRCEOC flag never becomes set. We have attached the code segment used to trigger the CRC operation and to subsequently start the Cortex-M33 boot process. Could you please review the implementation and confirm whether the initialization flow is correct?

void ConfigRetram(void)
{


/*********************
* 1 Enable ECC
*********************/
RAMCFG_RETRAM->ECCKEY = 0xAE;
RAMCFG_RETRAM->ECCKEY = 0x75;
RAMCFG_RETRAM->CR |= 0x01; // ECC Enable


/*********************
* 2 Hardware Erase
*********************/

// Unlock erase
RAMCFG_RETRAM->ERKEYR = 0xCA;
RAMCFG_RETRAM->ERKEYR = 0x53;

// Start erase
RAMCFG_RETRAM->CR |= RAMCFG_CR_SRAMER;

// Wait until erase is finished
while (RAMCFG_RETRAM->ISR & RAMCFG_ISR_SRAMBUSY)
{
valid_delay_ms(1);
}


FlashToRetram_Copy(0x00020000UL, 9150);


RAMCFG_RETRAM->CCR1 = 0x00; //Deactivate the CRC
RAMCFG_RETRAM->CR = (1<<12); //SRAMHWERDIS is set
//print_reg_info(&RAMCFG_RETRAM->CCR1);
RAMCFG_RETRAM->CCR1 |= 0x070; //128Kbytes
//print_reg_info(&RAMCFG_RETRAM->CCR1);
RAMCFG_RETRAM->CCR1 |= (0x01); //activate CRC
//print_reg_info(&RAMCFG_RETRAM->CCR1);
RAMCFG_RETRAM->CCR2 |= 0x01; //activate CRC
//print_reg_info(&RAMCFG_RETRAM->CCR2);

while ((RAMCFG_RETRAM->CSR & RAMCFG_CSR_CRCEOC) == 1)
{
valid_delay_ms(1);
}

 

/*********************
* 5 Read and Store CRC Signature
*********************/
crc_signature = RAMCFG_RETRAM->CCSR; // Read computed signature

RAMCFG_RETRAM->CRSR = crc_signature; // Write it to reference signature register

///*********************
// * 6 Finalize CRC Mode
// *********************/
RAMCFG_RETRAM->CCR2 |= RAMCFG_CCR2_CRCFC; // Clear CRCEOC flag

RAMCFG_RETRAM->CCR1 &= ~RAMCFG_CCR1_CRCC; // Clear CRCC bits
RAMCFG_RETRAM->CCR1 |= (0x2U << RAMCFG_CCR1_CRCC_Pos); // CRCC = 0b10 → CRC check mode



}



Additionally, we would like to know if an example project or reference application is available that demonstrates how to properly boot the Cortex-M33. If such material exists, we kindly request access to it.

Thank you for your support.

Best Regards

Akshitha Pattem

 

1 reply

ST Employee
January 7, 2026

Hi @Aks ,

You can find two examples based on CRC on STM32MP257F-EV1.
Here is the link:
STM32CubeMP2/Projects/STM32MP257F-EV1/Examples/CRC at main · STMicroelectronics/STM32CubeMP2 · GitHub.

In the 'README' files of these examples you can find how to run the code.

                                                                                                                                                                                      

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.