Skip to main content
Associate II
December 17, 2025
Question

secure-boot needs r/o rootfs, but post-install.sh rauc hook changes the rootfs after update instalaltion

  • December 17, 2025
  • 1 reply
  • 435 views

Hi everyone,

we applied the ST FWU reference solution on our own platform based on the STM32MP157F.
The solution was taken and adapted from the ST Yocto layer meta-st-ota (https://github.com/PRG-MPU-CUST/meta-st-ota).

In our setup rootfs must become read-only because of dm-verity application on rootfs requested by secure boot scheme.

Currently, making rootfs r/o is not possible because of post-install.sh rauc handler, which writes to the rootfs.


The problem, that after an update bundle installation, rauc calls the post-install.sh. This script edits MOUNT_PARTITIONS_LIST in the mount-partitions.sh script in rootfs of the next slot to mount correct `-a` or `-b` bootfs or vendorfs after the reset.

The solution that we think about, is to remove rootfs changing step from post-install.sh and to make mount-partitions.sh slot aware. 

 

Instead of mounting from MOUNT_PARTITIONS_LIST variable as-is, mount-partitions.sh should read the current slot from /proc/cmdline (rauc.slot=…), and based on that, decide whether to mount bootfs-a / vendorfs-a or bootfs-b / vendorfs-b.

What do you think? Is it a correct approach?

Maybe you can share patches for that?

It is hard to believe that nobody requested this change in the past (r/o rootfs is a common security need).  

thanks a lot!

1 reply

Christophe Guibout
ST Employee
December 19, 2025

Hello @maxim-senec,

 

I think your approach is correct.

FYI, the ST Yocto layer meta-st-ota is now public, and the URL has changed : https://github.com/STMicroelectronics/meta-st-ota

All new updates will be done through this layer.

So if you want to share some patches, feel free to use this new repository.


Thanks,

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.