Slow link up times with Gigabit Ethernet on the STM32MP1
I am testing Ethernet on the STM32MP1 (on both the EV1 and DK2 eval boards) and seeing slow link up times when the board is connected to a Gigabit Ethernet switch. Here's an excerpt from the dmesg traces showing link up times of 6-7 seconds:
[ 8.931934] Generic PHY stmmac-0:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=stmmac-0:00, irq=POLL)
[ 8.952777] dwmac4: Master AXI performs any burst length
[ 8.956664] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 8.964160] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 8.972895] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 14.169871] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/txSince my application does not really need Gigabit Ethernet, I tried limiting the speed to 100 Mbps in the device tree, as described here: https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration
However the results are still similar; typical link up times are in the ~6 second range.
Is there any way to shorten the link up times?
BR,
Guillermo